Part Number: OPA2343 As described above, my customer downloaded the opa2343 simulation model from ti.com, and then found that it's not virtual short with single +6v power supply, but it is virtual short under the practical test. And of course, the model…
Dan,
OPA2343, like most other op amps, does not have a ground pin; therefore, it may be used with single, dual, or asymmetric supplies with no change to its specifications. However, you must make assure that the input and output voltage ranges do not…
Part Number: INA333 Other Parts Discussed in Thread: OPA2343 , TLV2333 , OPA2333 , OPA391
Hi Ti team,
Please help to check the schematic below?
1,Differential signal input
Here is the schematic. Not sure it is being uploaded. There seems to be an issue?? Email might work better or I can send it to Daniel Carlson@TI
2438.CyberData PagingAmpSHT_SCH.pdf
Part Number: TPA3123D2 Hello,
Our company has been using this amplifier on three product with total part volume of at least 100K.
Recently we have had some returns for amplifier failure.
After further inspection at our facility, we found that the…
Hi Cedric,
Nope no firmware is required to establish the connection with emulator. You can once go through: F28335 controlCARD ZJZ Schematic [R2.2].pdf
Also, here are hardware guidelines:
Hardware Design Guidelines.pdf
Regards,
Gautam
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…