Part Number: OPA2349 Other Parts Discussed in Thread: OPA2349 I have an application which is attempting to use the opa2349 up to about 4Khz. My gain is relatively low: around 8, but it seems that the output is rolling off faster than I would have expected…
Other Parts Discussed in Thread: OPA2349 , OPA2369 Hi,
Could you provide the OPA2349 ESD rating information, our new part application system rejected this part because it didn't has ESD rating information.
Best Regards,
Giant
Hi Kevan,
Your OPA2349 die (chip) inquiry has been forwarded to our Marketing Engineering group for review.
Regards, Thomas
PA - Linear Applications Engineering
Hi Marek,
thanks.
Is OPA2348 also has the back-to-back input protection diodes? The issue came from OPA2348.
Another strange thing is that: When OPA2349 enter the "un-expect output status", once we use multi-meter to test the voltage between IN-…
Alessio,
I checked the data sheet for low current duals (in order) LPV802, LPV812, TLV8542, TLV8802, TLV8812, TLV522 , LPV542, TLV2402 OPA2369, LMC6442, TLV2369, and OPA2349. You can check higher ICC devices yourself if you like, but suspect over 30…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…