Part Number: OPA2354 Other Parts Discussed in Thread: TLV3542 , LMH6601 Tool/software: hi team,
my customer needs an amplifier with higher output current similar with OPA2354.Do u have some product to recommend? thanks!
Part Number: OPA2354 Tool/software: Can you tell me if the OPA2354 is "EMI hardened"? This part number comes up as such on a TI parametric search for EMI hardened op amps, but there's no mention of it being so in the datasheet. Thanks!
Part Number: OPA2354 Other Parts Discussed in Thread: TINA-TI Hi all
My customer is evaluating the OPA2354 for a low side current sensing function that should be fast.
They have this question:
What is the expected slew rate for a gain=11 ?
In…
Part Number: OPA2354
Hi
Customer would like to get the ROHS and TUV certification report for OPA2354AQDGKRQ1.
my email address is jack.cha@arrow.com
Thanks.
Part Number: OPA2354 Other Parts Discussed in Thread: OPA354 Hi, Team
From datasheet of OPA2354, the f-3dB is 250MHz(tested at G = 1), while GBW is 100MHz tested at G=10V/V(means f-3dB at G=1 should be around 100MHz, for a voltage feedback amplifier…
Part Number: OPA2354 hi dear supporting team,
my customer is using OPA2354 in their power module, circuit as below:
they need do short circuit experiment which will short the Vout poin in red circle below to GND for 1~2hours. when they short…
Part Number: OPA2354 Detail is as below and please kindly help to check and find out how to solve this problem,thank you~
1, using OPA2354 to amplfy IDR signal and SCH as below, Vcc=3.3V.
2,They found Voutb bias voltage is about 1V when testing…
Part Number: OPA2354 Hi
Please help with below question about OPA2354 V+/V-. Thanks!
Is it ok to connect V+ to GND and connect V- to negative 3V?
Regards
David
Hi Chentsu,
every OPAmp needs a minimum supply voltage to work properly. The internal circuitry (constant current sources, etc.) cannot work down to 0V supply voltage. That's impossible. The recommended minimum supply voltage of OPA2354 is 2.5V.
…