Part Number: OPA2365 Other Parts Discussed in Thread: OPA365 Dear TI Team
Our customer is considering OPA2365AIDR. Would you please teach me the impedance of the input terminals (No.2,3,5,6) of OPA2365?
Checking the following post, OPA365 states that…
Part Number: LMV321-N-Q1 Other Parts Discussed in Thread: OPA2365 , LMV321 , TLV6001-Q1 Hi,
I'm used LMV321-N-Q1 for PFC input voltage feedback.
OPA supply voltage is 3.3V.
When opa input is 110v, the output voltage be clamped arond 2.06v.
…
Part Number: OPA2365-Q1 Other Parts Discussed in Thread: OPA2365 Hello,
customer has to use OPA2365 (industrial) instead of OPA2365-Q1 because of delivery situation. Does both have the same electrical specification and where are the technical differences…
Hi Kai,
Thanks for your reply. From the first schematic, we can see that opa2365 was used as low side current sensing. So even the sensing current was 60A, the input voltage of opa2365 was 0.6V, which is less than supply voltage(3.3V). But from below…
Part Number: OPA2365 Dear TI Team
Our customer is considering the following circuit using junction resistor Rs and capacitive load CL for output at OPA2365.
Our customers are considering using it under the following conditions, are there any problems…
Part Number: OPA2365 Hello guys,
One of my customers is going to use OPA2365 for their new products.
At this moment, they have the following questions about OPA2365 absolute maximum rating
of input terminals. Could you please give me your reply…
Part Number: OPA2365 Hello Guys,
Good day.
Just like to confirm if the OPA2365 can be use for MRI applications?
Our customer is looking in particular on Non-magnetic opamps, but is this something TI have?
Thanks!
Art
Hi Rahul,
1. Are you talking about EMI rejection or amplifier noise? OPA2365 is much higher bandwidth, which may increase total amplifier noise, because you must multiply the input noise by sqt(bandwidth) to get total noise.
2. OPA2365 is a zero crossover…
Part Number: OPA2365 Other Parts Discussed in Thread: OPA838 Please help recommend parts related to OPA2365 specifications. I need to research 2nd source.