That recommendation is wrong; the TLV9101 is not a slow, low-power opamp.
The speed scales with power. Low-power alternatives would be the TLV2401/TLV6003 (5.5 kHz, 0.9 µA), OPA251 (35 kHz, 27 µA), or OPA244 (430 kHz, 50 µA). There is no reason to replace…
Part Number: OPA2251 Other Parts Discussed in Thread: LMC6462 , OPA251 , OPA2188 , LMC6482 Hello team TI, Need suggestion for the following:
The circuit outputs a DC current of 6.18nA when the input voltage VG1 is 1V.
What changes should I make into the circuit…
Hello Shimuzu,
I made a mistake in my previous message. The OPA241 is optimized for a low-voltage supply voltage and the OPA251 is optimized for a high-voltage power supply. Therefore the OPA241 features maximum offset and offset drift specifications…
Part Number: LMC6042 Other Parts Discussed in Thread: TLV27L2 , TLV27L1 , TLV2401 , TLV2381 , TLV2252 , TLV2451 Hello,
I am looking for other op-amps like LMC6042 with following requirements:
1) 10uA-20uA supply current
2) Vcc up to 26V
3) Input common mode…
Other Parts Discussed in Thread: OPA705 , OPA704 , LM317 , INA138 , INA210 , INA168 , OPA192 , OPA251 , OPA244 , INA282 , INA225 , INA270 , INA200 My application involves controlling fans to keep device temps within specs. I need to monitor high side current in this…
Other Parts Discussed in Thread: OPA2171 , OPA251 , OPA2251 , OPA227 , OPA277 , OPA244 , LM324 , TLV3702-Q1 , LMC6762 , TLV3702 I know this is long but please hang in there I need help on this please.
We are using the two op-amps in an OPA2171 as a window comparator…
Other Parts Discussed in Thread: UA741 , OPA251 , OPA244 , OPA241 , OPA237 , OPA211A , OPA211 I have a Ua741cp op amp and have noticed that it has a lower clamp of 2 volts and an upper clamp of -.5 volts from peak. I need to have a lower clamp of .5 volts or…
The TLV1805 eats 150 µA. The OPAx251 use a SOIC package. Gate drivers like the LM5112 do not support more than 0 V/14 V at the output. It appears you have already found your best choice.