Hello Andrew,
I am glad to hear the positive update from you. Asymmetric and unbalanced supplies do create oddities from time to time; please reconnect or ask more questions if you run into future issues.
Take care!
Best,
Alec
Part Number: OPA2670 Other Parts Discussed in Thread: OPA2673 , DEM-OPA-RGV-EVM Hi, does TI have evaluation boards that would work for OPA2670 or OPA2673?
Part Number: OPA2673 Other Parts Discussed in Thread: TINA-TI , OPA2675 Hello,
I want to define the DC voltage across the LED (Vanode - Vcathode) by 2.6V and then the signal comes over it with 400mVpp. Could you please help me to set the values? Increasing…
Part Number: OPA2673 Other Parts Discussed in Thread: OPA2677 Hi,
Could you let me know below sequence is available?
1. MCU GPIO --> A0/A1
2. 12V supply V+, GND V-
Thanks.
Part Number: OPA2673 All,
I have seen SBOA120 and was wonder if there is a similar app note using capacitive coupling; I am coupling a low data rate signal onto AC line for PLC.
Thanks,
Regards, Joe
Part Number: OPA2673 Other Parts Discussed in Thread: OPA2832 , LMH6612 , LMH6639 , SN74BCT25244 , LMH6611 , OPA356 Hi
We are planning to use OPA2673 for our application which have two opamp channels, we are planning to use these two channels as per below…
Part Number: OPA2673 Other Parts Discussed in Thread: OPA2677 , OPA2670 , THS6301 To whom it may concern,
I wonder if the two 1/2 amplifiers in OPA2673 are designed only to operate in a differential fashion, or can I just use 1 of the 2 amplifiers, with…
Part Number: OPA2673 We recently shipped over 250 products including the OPA2673 from Belgium into Spain by road transport (Barcelona, then further to 23 different sites). Once arrived, on all sites, 90% of the products showed degraded performance. After…
Part Number: OPA2673 To whom it may concern,
I just want to confirm about the connections of NC pins and PowerPad.
Can NC pins be left unconnected?
Must PowerPad be connected to VS- or can it be left unconnected? (I have this doubt because PowerPad is…
Part Number: OPA2675 Other Parts Discussed in Thread: OPA2677 , TINA-TI , THS6222 , OPA2673 Hello,
I am going to drive a 100 Ohm twisted pair line. The input p-p voltage is around 100mV and I would like to amplify it am much as possible to keep the 100 MHZ…