Part Number: OPA277 Hello, this is Moon.
I am currently using the OPA277 as a buffer. The datasheet provides the output impedance only up to 1 MHz, but I would like to know the output impedance around 200 MHz. My rough estimation is in the range of…
Part Number: OPA277 Other Parts Discussed in Thread: OPA2192 hi,
we are using OPA 277 U K part in our board as a unity gain amplifier. In which we are facing problem at low voltage input. When input at pin 3 is 0.635V , at pin 6 (output) we get zero…
Part Number: OPA277 Tool/software: Please check the below part, we received marking - not sure it's correct marking.
CPN: COB24-205189-277
PO SPO016220
Assembly site code : A = ?
Assembly site code : K = ?
Spec datasheet: OPA 277U A…
Part Number: OPA277 I downloaded the Noise Calculator from the TI website to calculate the noise of a non-inverting amplifier. I also watched the TI Precision Labs Noise videos.
In the video, it is explained that to obtain the output noise voltage,…
Part Number: OPA277
Could you clarify the difference between the OPA277P’s two “ Offset Trim ” pins and a traditional “ Offset Null ” pin? Specifically, are “offset trim” and “offset null” equivalent terms that can be used interchangeably on schematic…
Part Number: OPA277 Hi exparts,
Could you tell me the behavior of a voltage follower circuit of OPA277 with non-inverting input? Settle at a certain voltage, become undefinded, or oscillate and so on.
Regards, Hiromu
Part Number: OPA277
How would you test for this op amp's open loop output impedance vs frequency and dc physically? Are the inductor and capacitor there only for simulation or are small values needed in real life? And how would you apply a current …
Part Number: OPA277 Tool/software: Hi expert, We want to promote TI's devices to replace OP177GSZ-REEL7 (ADI), could you help to recommend TI's suitable devices? Thanks.
ADI-OP177.pdf
Best Regards,
Ryker
Part Number: OPA277 Tool/software: Hello,
We received the part OPA277UA/2K5 from DIGIKEY but the marking is OPA277U K instead of OPA277UA.
Can you please let me know what is the “K” and “A” represents In the MPN ?
Thank you in advance
Best re…
Part Number: LMH6704 Other Parts Discussed in Thread: OPA277 , , OPA855 Hello,
I’d like to ask about two TI op amps (LMH6704 and OPA277) and some behaviors I’m observing. There are two main questions.
Common system / measurement information - Supply…