Part Number: OPA2828 Other Parts Discussed in Thread: JFE150 , OPA928 , OPA205 , OPA227 , OPA277 , OPA627 , OPA211 , OPA828 The TDS provides a voltage noise spectrum which is helpful. I would like to see a current noise spectrum too, not just the current…
Part Number: OPA2828 The datasheet (p. 5) specifies the parasitic capacitance of the input impedance as 6 pF.
I want to know variation of the parasitic capacitance in the input impedance.
If there are any measurement data on the variation of parasitic…
Part Number: OPA2828 Other Parts Discussed in Thread: OPA828 Tool/software: Hello,
Is the OPA2828 available in an 8 pin D-type package? Or is it only available in the DNG package?
I am worried about hand soldering the thermal pad on the DGN package…
Part Number: OPA2140 Other Parts Discussed in Thread: OPA2828 , OPA2156
Tool/software:
Hi experts,
Could you pick up some recomended opamps which have higher frequency and lower noise than OPA2140 as a replacement? My first thought is OPA2828. …
Part Number: OPA140 Other Parts Discussed in Thread: OPA2828 Hi Experts,
Can you help with the inquiry below?
I have to design a charge Amplifier for a piezoelectric Sensor. The sensor capacity is between 30 and 50 pC, amplification should be at least…
Part Number: DAC8811 Other Parts Discussed in Thread: OPA2828 Tool/software:
This is a test board we made based on the TI DAC8811 development board, where C2, C3, and R5 were not soldered
This is the timing sequence of CLK, SDI, CS
for(i=0;i<36;i…
Part Number: OPA2210 Other Parts Discussed in Thread: OPA2211A , OPA2828 , OPA2189 Hi TI,
I am looking at an application, in which OPA2210 can meet almost all requirements, except its slew rate. Do you have any part suggestions? I need ~3x OPA2210 slew…
Part Number: OPA2210 Other Parts Discussed in Thread: OPA2140 , INA851 , OPA2828 , PGA855 , OPA140 Tool/software: The previous thread was locked.
I stacked another resistor network on OPA2140 feedback, and the CMRR improved. The unit is in uV/V
…
Part Number: TPS7A33 Hello
My TPS7A3301RGWT was purchased through an official channel, bought at JLC in Shenzhen, China, and had SMT assembly done there.
Circuit Description:
Two TPS7A3301RGWT and two TPS7A4701RGWT share a ±22V linear power supply…