Part Number: OPA2863 Hi Team
Greetings! Could you pls take some time to confirm this issue and give me some advice?
The OPAx863 (only found on the OPA2863 product page, not the OPAx863 product page?) model has some problems. The most obvious of which…
Part Number: OPA2863 Other Parts Discussed in Thread: LMH6643 , Tool/software: Hi Sir,
My customer use OPA2863 to replace LMH6643 for one year. Application about the circuit is 4 level inverting amp application (using 2 OPA2863). The first input signal…
Part Number: OPA2863 Other Parts Discussed in Thread: , OPA2626 Tool/software: Kindly provide below tech spec for part OPA2863IDGKR
Input Capacitance Differential Mode
Input capacitance Common Mode
Input Resistance Differential Mode
Input Resistance…
Part Number: OPA2863 Other Parts Discussed in Thread: LMH6643 , Hi Sir,
Customer want to replace LMH6643 by using OPA2863 due to LT question. They test sample and buy a reel OPA2863 for replacement test but have high failure rate / burn out issue.(Failure…
Part Number: OPA2863 Other Parts Discussed in Thread: TLV1811 Hi Team,
I am simulating OPA2863 as a comparator. Below is the schematic.
The voltage at IN i.e after the resistor divider output is 1.5V. It increases only after the expected resistor…
Part Number: OPA2863-Q1 Other Parts Discussed in Thread: TLV1832 Tool/software: Hi Team,
I am looking for the op-amp. which can act as comparator with the below specification.
Vin= 3V to 30V
Vout= 2V to 9V
rail to rail output
Qualification:…
Part Number: OPA2863
Dear TI:
I am using part number OPA2863RUNR as a buffer amplifier. This amp features a power-down pin. The amplifier IC package is powered with 5VDC.
I am observing that when the power-down pin is above 3.9VDC the output buffer…
Part Number: OPA2863 Other Parts Discussed in Thread: OPA2837 Dear TI:
I am using part number OPA2863RUNR as a buffer amplifier. This amp features a power-down pin. The amplifier IC package is powered with 5VDC.
I am observing that when the power…