Part Number: OPA2863-Q1 Other Parts Discussed in Thread: TLV1832 Tool/software: Hi Team,
I am looking for the op-amp. which can act as comparator with the below specification.
Vin= 3V to 30V
Vout= 2V to 9V
rail to rail output
Qualification:…
Part Number: OPA863 Other Parts Discussed in Thread: OPA2863-Q1 Tool/software: Hi, Support Team
about OPA863, do we have same function for Automotive parts?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Written by: Charles Barsh
The electrification of automobiles is rapidly increasing, and as it does, there are more advanced systems integrated into these vehicles. These electrified vehicles contain sensitive GaN and SiC switches that are susceptible…
Part Number: TLV3502-Q1 Other Parts Discussed in Thread: TLV3502 , TL431 , OPA2863 Hi,
I am facing a issue, with TLV3502 comparator circuit block. When the high threshold comparator latches the output to 0 logic and high logic I get voltage dips at…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…