Girish,
Please go to www.ti.com/.../toolssoftware and download the OPA314 TINA-TI Spice Model. Unzip that and you will see a file called OPA314.lib. This is the SPICE netlist of the OPA314 model. You can import this file into MultiSim.
Here's a…
Other Parts Discussed in Thread: OPA314 , TLV314 , LMV651 , OPA341 , TLV2422 The OPA314 is designed into a strain-gauge monitor and performs to the requirements, however, the Iq is too high. Would like a drop-in replacement wit lower Iq, and the following…
Thank you very much, Marek - very helpful!
It is said often these currents double every then degrees, but there are (and will be more) exceptions.
For example look at MAX9914: also an CMOS amplifier but I_bias really is different from OPA314.
I…
Other Parts Discussed in Thread: OPA627 , OPA314 , TINA-TI Hi all Would you mind if we ask OPA314 ? Our customer mesured En and there was some difference between the datasheet and their measured value. -Measured value : 20~21nV/√Hz(1kHz~10kHz) -Datasheet…
Other Parts Discussed in Thread: OPA314 , OPA348 Any experts out there know what it would take to convert the OPA314 TINA model into a workable Spice model? I'm using OrCAD 16.5 and the TINA model for OPA314 causes no errors, except convergence errors…
Other Parts Discussed in Thread: LMV851 , LMV831 , OPA314 , OPA376 I'd like to talk regarding a IC which has compatibility with NCS2004 and lower height than NCS2004.
Please let me know the riight person who can talk about this with me.
Thanks and…
Other Parts Discussed in Thread: LMV551 , OPA314 Hello,
I am looking to understand physical pressure induced characteristic changes in reagrds to the the following two Op Amps:
LMV551MG/NOPB and OPA314AIDCKR (SC70 Pacakges).
The circuit containing…
Part Number: ADS1015 Other Parts Discussed in Thread: OPA314 I have a question on the stability of a design using the OPA314 and ADS1015. There will be a differential signal to the OPA314 inputs, and the output will go to ADS1015.
Schematic
Do you…
Part Number: OPA313 Other Parts Discussed in Thread: OPA316 , OPA314 , , TINA-TI Current issue is that I am comparing some circuits using OPA313, OPA314, and OPA316 pspice models. If I simulate identical circuits using OPA313 and OPA314 in the same schematic…
Hi Raymond,
Thank you so much for your answer!
Actually I have no idea what I should do because I have no experience choosing the appropriate component.
I don't know what should be taken into consideration from the datasheet.
Can you please tell…