Other Parts Discussed in Thread: OPA316 , OPA827 [ OPA316 ] General Questions, Gain, Gain Error/Flatness
Hi, Sorry that it's not specific question related to OPA316. However, if I draw the relationship between input and output voltage as below, * Gain…
Other Parts Discussed in Thread: OPA316 , TIPD154 , OPA317 1. I have application where input signal voltage varies from +5V to -5V. Have to level shift the signal and fed it to microcontroller adc which is sampling at 1MSPS. Microcontroller adc range varies…
Good morning Wei-Hao,
Yes, the TLV316 does not show a max drift spec,
It is however a relaxed limit version of the OPA316, which does show a max,
Roughly speaking the drift is proportial to the 25C offset voltage, so - if the test limit has increased…
Hello, the selected device should work fine with the OPA316, as a reference of the output ripple you can have a look at figure 18 in the d/s. We don't have any output noise measure in the d/s. You can also consider the tps62740 if low Iq is a feature that…
Hi Ron,
Yes, the variance matters more because customer doesn't want few failure due to the large variance in mass production, maybe the device such with max value such as OPA316 and OPA322 is more reliable, we will try these two devices first.
Thanks…
Part Number: LMV951 Other Parts Discussed in Thread: TLV316 , Hello support team,
My customer would like to use LMV951 as charge amp and achieve same gain/phase performance with Vcc 1.3V as TLV316. However, the performance looks different from TLV316.…
Part Number: TLC4502 Other Parts Discussed in Thread: OPA2335 , OPA2325 , LMP2022 , LMP7721 , OPA2316 , OPA320 , OPA325 , OPA316 Hello everyone.
I am looking a replacement for TLC4502. Any recomendations?
Thanks!
Thanks Tim, that's good to know. Both the OPA313 and OPA316 have been updated recently and are running our latest model architecture, so I'm glad to hear that the results agree in both tools.
I'm going to send you a friend request, let's take…
Dear Ahana,
Thank you, you just demonstrate that the LMP7731 does not converge correctly. The OP of your simulation is completely wrong. A simulation that run to the end does not mean the result is correct.
Here is the simulation with an OPA316, a model…
Part Number: LMV722 Other Parts Discussed in Thread: OPA316 , TLV9062 , TLV2172 , OPA2172 , LMV721-N , Hello, customer ask for PSPICE model for the LMV722.
Regards, Holger