Other Parts Discussed in Thread: OPA317 , OPA333 Do you have a EMIRR IN+ vs Frequency graph of OPA317? There is this data for OPA333 in OPA333 EMI Immunity Performance.
Best regards, Y.Hirata
Other Parts Discussed in Thread: MSP430F4152 , OPA317 , OPA330 , XTR117
My MCU is MSP430F4152 current consumption 0.5mA use PWM to Iin RC to Iin use 12K resistance ,But i test IO pin current is 4.12mA i change PWM duty cycle but 4.12 is minimum, i do…
Shreenidhi,
The specified OPA317 input common-mode voltage range is 100mV beyong the rails, which in your single supply application, with Vs=5V, means from -0.1V to 5.1V - see below.
Let me first bring it to your attention that your circuit might be…
Other Parts Discussed in Thread: OPA316 , TIPD154 , OPA317 1. I have application where input signal voltage varies from +5V to -5V. Have to level shift the signal and fed it to microcontroller adc which is sampling at 1MSPS. Microcontroller adc range varies…
Other Parts Discussed in Thread: OPA4317 , OPA317 , TINA-TI Hi,
In a design I am using OPA4317 as unity gain buffer. I am using single supply 3.3V. I want to drive 0.1uF capacitor with it, what should be the value of isolation resistor so that this design…
Hello Tarun,
You can replace the OPA317 with the LM358 in the circuit featured in the reference design: TIPD158
As mentioned before, consider using the XTR117 which integrates many elements of the circuit featured in TIPD158 .
Other Parts Discussed in Thread: OPA317 Hello. I need to design a circuit with the following specifications.
Input varies from 0-12V
For input varying from 0-10V, output should vary linearly from 0-5V.
For any input more than 10, output should get saturated…
Other Parts Discussed in Thread: INA148 , INA326 , OPA317 , INA331 , INA332 Hello,
I am looking for differential amplifier with vref and high input resistance at the Vref input (would like to use resistors to set the voltage with minimal current )
can you…
Other Parts Discussed in Thread: XTR117 , XTR115 , OPA317 , XTR116 Hello-
I am having an issue with an XTR 115 breaking into oscillation when doing a step function from 4 to 20 mA. This oscillation can be seen on pin 5, 6, and to a lesser degree, pin 7. I…