Part Number: OPA376 Other Parts Discussed in Thread: TLV376 , , LM7705 , OPA340 Hi Team,
customer has done some simulations with OPAx376 and TLVx376 in LTspice.
They noticed that the output does not go below 10mV for both devices.
Would you know what might…
Part Number: INA331 Other Parts Discussed in Thread: OPA340 Hello,
Q1.
I am planning to use a DIGITAL POTENTIOMETER at the P1 location in the circuit to adjust the gain of INA331. The output range of INA331 is -1V to 1V. Is it acceptable to use a DIGITAL…
Part Number: OPA2340 Other Parts Discussed in Thread: OPA340 Hi,
Can you clarify the Operating temperature range on the OPA2340. On the web page it states -40 - +85C and in the data sheet under 6 Specification it states in multiple places -40 - +125C …
test5.rar
Hello Marek
I have already connect the other point of the Rogowski Coil to 1.5V. So the offset voltage is not from OPA340.
I guess the problem is from the R/C integral and the protection diode. I attach my simulation file in Pspice.
When I disconnect…
Other Parts Discussed in Thread: OPA340 , OPA353 , OPA350 , ADS7816 Dear TI empployee.
We don't use RC network filters as shown below.
1. If we don't use RC network filters problems.
2. I know that OPA340 serise optimized for driving medium speed…
Other Parts Discussed in Thread: OPA340 , OPA365 OPA340MDBVTEP and OPA365MDBVTEP
What operational limitations might there be to measure signals within 1 to 5 mV from the lower rail on the input? The amp is strapped to a gain of 24 so the output signal…
Other Parts Discussed in Thread: OPA340 , OPA340-EP Hi team,
considering OPA340-EP, we were wondering if we might have there too some TINA or PSpice models available, as per standard OPA340 so far.
Thx in advance for kind comments and BR
Sergio Fa
AskTexas…
Other Parts Discussed in Thread: OPA340 , OPA350 , THS4521 I see in the datasheet of OPA340, it is suitable to drive a 100kHz sampling converter. I would like to know whether it could be used in even high speed converter.
How to do the analysis?
Thank! …
Other Parts Discussed in Thread: OPA340 Hi all. I would like to know the following absolute values of OPA340. ・Pd(mW) ・Sink and Source Current of output pin(mA) Best Regards, Sho Ogane
Other Parts Discussed in Thread: OPA340 Hi guys! we're working on OPA340 for an rectifier. We config it as a superdiode with single supply, but when we apply a negative voltage to the positive input, the output reflects the negative inout voltage (up to…