Part Number: OPA348 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hello,
I dont think I am getting the right output when I try to induce an offset.Please see the file attached. The offset seems to be 2V instead of 1V. …
Part Number: OPA348-Q1 Hi Team
using OPAMP, I would like to make Shunt Amplifier to measure a current.
the output will be affected by DC Offset and Offset Drift over temperature and Gain error.
I can estimate worst case of DC Offset and Offset Drift…
Part Number: OPA348 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi team,
I have a question regarding the functionality of the time-controlled switch. I'm trying to replicate a load step response on an LDO output, but…
Part Number: OPA348-Q1 Hello team,
My customer have a question. please review below question and let me know your opinion.
1. Bypass capacitor : Which value is correct? 0.1uF or 0.01uF? - Datasheet section 7.3.1(12 page) Power supply pins should be bypassed…
Part Number: OPA244 Other Parts Discussed in Thread: TLV2451 , , OPA348-Q1 , TLV2381 , OPA347 , OPA348 Hi all Would you mind if we ask some opamps? About below amps, which amps are JFET or bipolar type? We are sorry that we could not judge correctly. As our recognition…
Part Number: OPA348 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models I am using OP348 in one of the circuit and while simulating in LT Spice getting this error "u1:vccvs1_in: Missing value, assumed 0V @ DC" in Spice Error…
Part Number: OPA348-Q1 Other Parts Discussed in Thread: OPA4348-Q1 , , OPA2348-Q1 , OPA2348 , OPA4348 , OPA348 , TLV3701 , TLV3702 , TLV3704 Hi Team
my Customer has the following questions about FIT for OPA348-Q1/OPA2348-Q1/OPA4348-Q1.
may I expect your swift…
Keith,
OPA348 clearly shows the 1/f input voltage noise spectral density - see Fig 17 datasheet; it is 35nV/rt-Hz @ 1kHz and 650nV/rt-Hz @ 1Hz. There is, however, no 1/f input current noise that is typical in CMOS op amps.
Other Parts Discussed in Thread: OPA2348 , OPA4348-Q1 , OPA348 Hi Team
inOPA348-Q1(OPA2348/OPA4348-Q1) datasheet,
there is no comment on the Abs Mas voltage for the differential input voltage.
may i know it ?
Mohammed,
Who is the person who put U5B TLV4376 in the current zero and U2 OPA348 in the voltage zero? These two circuits make zero crossing harder to detect. They are completely unnecessary for zero cross. Can these two circuits be removed or the zero…