Other Parts Discussed in Thread: OPA692 , OPA355 , OPA357 , OPA358 , OPA361 , OPA360 , OPA362 , TL592B , UA733 , LMH6570 https://www.rohm.com/products/audio-video/video-amplifiers/isolation-amplifiers/bh7673g-product
Hi Teams,
I would like to searching…
Hello Amruta,
I can help you with the OPA355 and OPA343 op amps. Note that the HBM and MM numbers are the same for the various suffixes you listed:
OPA343 HBM 500 V MM 100 V
OPA355 HBM 4 kV MM 500 V
The DIT4096 is a digital audio transmitter and…
Hi,
I see we don't have a spice model available for DAC5662 which can be simulated in TINA-TI. Sorry for the inconvenience caused.
Regarding LMH6618 & OPA355 you can get the spice models under "Design and Development" Tab of respective part number…
Other Parts Discussed in Thread: LMH6629 , OPA355 hi, everyone.
I am using LMH6629 as TIA(trans-impedance Amplifier).
BUT it seems not work. my application is : receiving infra-red signal(wavelength~900nm), bandwidth range from 2 to 8MHz.
I can…
Dear Mr Hooman,
Thanks for the reply on OPA656. We are using OPA358, with INA122, and the the 1550NM PD and IRLED. WE ARE finding difficulty in using OPA358 CAN U PLS. confirm if OPA355 WHICH u have suggested will solve our problem. can we replace OPA355…
I have not found any models for the OPA356, however there are models for OPA355, which is the same as OPA356 but with lower VIO and shutdown. The models can be found in the product folder:
http://www.ti.com/product/opa355
Rachel
Andrew, you probably should not be switching to a non-RR out device like the THS4211, here are your choices in RRout, higher slew rate VFA devices from TI or NSM, Be careful with those SSBW for the CMOS parts - those are false high numbers not even remotely…