Hi Marcel,
If we look at the abs max table of the OPA2356, the device's abs max operating temperature is -55C to 150C:
However, the specified temperature is -40C to 125C:
A different way of reading this is that the device will not break if inside…
Hi Luke,
First check all of the distributors. Second, the OPA365-Q1 and OPA365-EP are the same device, they just have more intensive vetting which adds cost.
We have two alternatives available: OPA607 and LMV793 aka LMP7717. These can be externally…
Part Number: OPA365-Q1 Other Parts Discussed in Thread: OPA365 , OPA365-EP , LMV793 , OPA607 , LMP7717 , OPA354 Hello,
Is the OPAx365-Q1 equivalent to the OPA365 except the OPAx365-Q1 is qualified for automotive?
We have used the OPA365 with excellent…
Other Parts Discussed in Thread: OPA2365 , OPA2350 , OPA365-EP , OPA365 , TINA-TI , OPA320 , OPA369 , OPA364 , OPA350 Hi,
I have a TIA design that uses a OPA2365. The schematic is shown below.
The TIA function performs well over the bandwidth of interest…
Performance at -55C is not guaranteed. The EP version undergoes extra testing to ensure performance is met. I would not recommend using the non EP OPA365 at -55C.
Part Number: ADS8548 Other Parts Discussed in Thread: ASH Hi,
I am having plan to use the ADS8548 for space application. This component is on the list of the space and defense datasheet of the TI document that it is attached."slyc143e.pdf".
In the…
Part Number: DLP3021-Q1
Dear team,
1.Is there a datasheet for PHOTODIODE used by P07? What are the placement requirements for this PHOTODODE in practical applications? Can this part of the circuit be removed in the application of puddle light…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…