Part Number: OPA4170 Tool/software: HI
kindly check below photo and confirm which are the components belong to? You can chose A, B, C,D,E, or F.
Kindly confirm back to me with today, thanks a lot.
Part Number: OPA4170-Q1 Hi..
I want to design a op-amp circuit, with single output pin.
Input :- 0V to 5V
Output:- -10V to +10V
at 0V input output will be -10V and 5V input output will be +10V
Part Number: OPA4170-Q1 Other Parts Discussed in Thread: OPA4170 , OPA4991-Q1
I have asked from my customer regarding difference between OPA4170-Q1 and nonQ1 product.
I recognize the difference difference between OPA4170-Q1 and nonQ1 product is specification…
The LM2902 can output voltages near GND only if the load is not too high.
Quad R2R-output opamps with similar paramters are the TLV9304, TLV4170, OPA4170, or OPA4990.
Part Number: OPA4170 Hi,
A capacitive load is connected to the 3 channel output terminal of the OPA4170AIPW.
When the short-circuit current of the output terminal was measured, it was confirmed that the waveform of the short-circuit current of about 20…
Part Number: OPA4170-Q1 Other Parts Discussed in Thread: ISO7740 , OPA170 I recently tried running a SPICE simulation using the model for OPA170 op amp. Positive input is fed from ISO7740 device where voltage transitions from low to high. Negative input…
Part Number: OPA4170-Q1 Other Parts Discussed in Thread: OPA2990 , OPA4170 Besides the 40V absolute max rating for supply voltage (single supply configuration) for this device, is there any information on the abs max rating for transient conditions? I…
Part Number: OPA4170-Q1 Other Parts Discussed in Thread: OPA4170 , OPA4171 Hi champs,
My customer evaluated OPA4170 and OPA4171 with attached circutry.
As shown in attached file, when OPA4710 was applied, output sinsoidale waveform shows distortion, but…
Part Number: OPA4170 Hello,
When I think output voltage vs output current for the OPA4170 with Negative feedback loop...
Should we refer the Voltage output swing from rail in Electrical Characteristics?
Or is it for open loop and should we refer Figure…
The TLV9104 is a mainstream product, but it is cost optimized and has a slightly higher noise. The TLC2264 is still good at what it does.
Comparison of TLC2264, TLC2274, TLV9104, OPA4170 .