Part Number: OPA4192 Other Parts Discussed in Thread: PSPICE-FOR-TI Tool/software: Dear Members,
I simulated a complete circuit using TI-TINA 9.2.30, and now I want to migrate to PSPICE-FOR-TI. Is it possible, or do I need to redraw the circuit completely…
Part Number: OPA4192 Other Parts Discussed in Thread: OPA192 Tool/software: Hi,
I can't find the ibis model for the OPA4192 component on your website.
Is there an alternative model that I can use?
Thanks,
Linh
Part Number: OPA4192 Tool/software: Hello, This is Kwonjoon Lee from South Korea.
(Question)
1. I would like to ask if I can apply 0V and -10V to the positive power supply (V+) and the negative power supply (V-) of the OPA4192, respectively.
Best regards…
Part Number: OPA4192 Other Parts Discussed in Thread: OPA547 ,
What is the maximum voltage that can be shorted to the outputs of the OPA4192 and OPA547 from an external power supply that is referenced to the internal PS ground? Currently there is no specification…
Hi John,
That is too bad that the leadless package is disallowed for this design. Otherwise, I think the INA851 would be perfect if you can budget the additional Iq, 7mA (max @25C) vs 4.8mA (max @25C) for OPA4192.
John Gray said: So, then I would ask for…
Part Number: OPA4192 Good Day. The OPAx192 pspice model that was downloaded from TI.com has issues at times when running on a single supply (like 5V to ground). it looks like it's taking time while computing bias levels. Is there a recommended option…
Part Number: OPA4192 Other Parts Discussed in Thread: OPA192 Good Afternoon,
I'm wondering if someone can help me define the min and max of the settling times slew rate limits for the OPAx192 Op amps. There are typical shown but not the extremes. …
Part Number: OPA4192 Other Parts Discussed in Thread: OPA4387 , OPA4376 Hi Expert,
Customer found output noise issue with OPA4192.
Circuit : voltage follower.
V+=5V, V-=0V
This noise seems to come from power supply noise(1MHz). It has same frequency…
Hi Art, Thanks for the response, that helped.
A follow up question.
So for the multi amp packages, OPA2192 and OPA4192, if one amplifier shorts to ground and goes into thermal protection, does that cut power off to the entire chip or just the amplifier…
Part Number: OPA2192 Other Parts Discussed in Thread: OPA4192 Tool/software: Hello. This is Kwonjoon Lee from South Korea.
I would like to ask about the absolute maximum ratings in power down of OPA2192 (or OPA4192).
(Detailed Situation)
1. In my power…