Hello Michael,
I searched the web for DIP adapters that would accommodate modern dual and quad SOIC packaged op amps. The LM3900N pin out is so unique I didn't find any DIP adapter that would work. I thought the old TI RC4136 quad op amp used the same…
Hi Rico,
Do expect that any op amp I suggest should be evaluated in your system to make sure it meets all the electrical performance requirements.
Since you require a quad op amp that can operate with +/-3.3 V supplies and fast overload recovery,…
David,
We have several quad op amps with the input common-mode voltage range beyond both rails; please see take a look at OPA4191, OPA4192, OPA4196 and OPA4197.
Hi Charles,
I know what is going on. You are applying the OPA4188 amplifier section as a comparator, with a 2.21 V reference voltage applied to the inverting input. When you drive the non-inverting input to the 1.45 V level you forward bias one of the…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…