Part Number: OPA544 Tool/software: Hi TI experts,
We aim to control the output current via the input voltage, as illustrated in the figure. While the ideal output current should have no DC offset, an offset current is introduced due to the input offset…
Part Number: OPA544 Tool/software: Hi TI Team,
Our customer requested the ESD please help to provide it.
Material name : OPA544F/500
Best regards,
Takako Fujiya/TED
Part Number: OPA544 Other Parts Discussed in Thread: OPA548 HI Sir
I use opa544 as a voltage source to test the DUT. There will be current measurement circuit between the lines. Sometimes the current circuit will oscillate, But when replaced with OPA548…
Part Number: OPA544 Tool/software: Hello E2E Experts,
Good day.
On page 2, Figure 1. Battery Simulator Circuit, the BAT+ terminal on the right side output, the reference for the OPAMP at the top listed as -12V . Is this the correct polarity?
Same…
Part Number: OPA544 Other Parts Discussed in Thread: OPA2544 Hello?
As title, I would like to inquire because there is a discrepancy in the temperature information.
In datasheet of OPA544;
DESCRIPTION in page 1 - It is specified for operation…
Part Number: OPA544 Hello,
We apply the two package of OPA544 as a emmitter follower.
Under no load condition, the power consumption of OPA544T is about 100mA , and OPA544F is only about 25mA.
we would like to ask if the power consumption of OPA544T…
Part Number: OPA544 Other Parts Discussed in Thread: BQ24090 , BQ24157 , The Below app note which is "Building Your Own Battery Simulator" App note by TI, I have few queries on the same,
My battery: single cell, Battery not decided yet, but it will…
Part Number: OPA544 Dear team,
I am using OPA544 OP-amp to build gain amplifier. To power-up Op-amp i have positive 60V DC power source.My question is ,
1. To power-up OPA544 should i need both positive and Negative voltage ? or will it work only…
Part Number: OPA544 Other Parts Discussed in Thread: OPA549 , OPA548 , Good afternoon,
I have been looking at the document entitled, "Building Your Own Battery Simulator" (Application Report SLVA618–October 2013) I would like to make use of this idea…
Part Number: OPA544 Hi Raymond,
We have performed tests with the circuit recommended by you (attached with the component value changes) with the change of the L&C values.
L & C Values recommended: 10mH & 1uF
L & C Values used in the circuit: 1…