Part Number: OPA547EVM Other Parts Discussed in Thread: OPA549 Tool/software: Hello, is there a similar EVM available for the OPA549? Even Gerber files would be enough to work with, no need for a finished EVM product.
Best Regards, Johannes Mathieu
Part Number: OPA547EVM Tool/software: I'm not a EE and I'm a little unsure how to interpret table 4 in the user manual. If possible, I would appreciate a photo, or Figure 2 marked up to clearly indicate the physical jumper positions that correspond to…
Part Number: OPA547EVM Other Parts Discussed in Thread: OPA547 Dear TI engineers
I would like to use the improved Howland circuit using the OPA547EVM PCB. my purpose is to drive a MEMS resistor of a few ohms typically from 10 to up to 500 ohm or even…
Part Number: OPA547EVM Other Parts Discussed in Thread: OPA547 following my previous request , i d like to drive current between 10 to 200 mA to heat up in AC a few ohm resistor. thanks
Hi Ahmed,
what do you want to tune? The load or the feedback resistances?
The feedback resistances don't need a tuning, provided you are using 0.1% resistors.
Kai
Part Number: OPA547EVM Other Parts Discussed in Thread: OPA547 , TINA-TI , OPA548 , OPA551 , OPA548EVM , Hello,
I am a mechanical engineering student, and I considering using the OPA547/OPA 548 Evaluation Module as a current amplifier, the input will…
Part Number: OPA548EVM Other Parts Discussed in Thread: OPA548 , OPA547 , OPA547EVM Hi BU,
My customer is using OPA548EVM and would like to know the exact specs for resistive, capacitive and inductive load.
I couldnt find this information in datasheet…
Part Number: OPA547 Tool/software: Dear All , I am using the OPA547 to amplify a 3V AC signal to 20,5V AC. I followed the Improved Howlannd Current pump circuit described in the below schematic. (You can find it in this document OPA547EVM, OPA548EVM User…
Part Number: OPA548EVM Other Parts Discussed in Thread: OPA548 , OPA547EVM , OPA547 , OPA549 , OPA541
Part Number: OPA548EVM
Other Parts Discussed: OPA548, OPA547EVM, OPA547
Hello TI Support,
I would like to use the OPA548EVM as a linear…
Part Number: ALM2403-Q1 Other Parts Discussed in Thread: OPA547 , OPA593 , OPA547EVM , OPA593EVM Tool/software: I did purchase ALM2403-Q1 dual-power op amp.
Connections made:
pin 1 : NI FPGA GND
pin2: NI FPGA Analog output ch1
pin10: +12V
pin…