Other Parts Discussed in Thread: OPA992 , OPA2613 , OPA552 , LM7171 , OPA2156 , OPA2992 I am searching for an op-amp with the specifications mentioned below,
slew rate >= 30v per micro second
output current >= 100mA(at least it should be greater than…
Part Number: CD74HC4051 Other Parts Discussed in Thread: OPA552 , , MUX36S16 , MUX36S08 Hi, guys. The CDx4HC405x, CDx4HCT405x has Input Voltage Range: ±5-V Maximum.
I'm using an OPA552 Op Amp with +/- 30V dual supply for creating +/- 30V output signals…
Hi Sayali,
Can you help me understand the intended use case for this? What is this AC output driving? Is the precision of frequency important? Or does the frequency just need to fall within 4-6kHz?
How important is efficiency? If not too important…
Other Parts Discussed in Thread: OPA552 Dear Sirs
Does TI provide High-Voltage, High-Current Operational Amplifiers solution like O PA552 (could support 60V) and cheaper solution (cheaper than OPA552)?
Thanks
BRS
Nat
Part Number: TPS61390 Other Parts Discussed in Thread: OPA552 , , TPS61175 , TPS55340 Hi, I'm using +-30V high voltage OPA552 Op Amp from TI. I have used this Op Amp with an external power supply until now.
However, I have to make this as a battery…
Hi Thomas,
First of all a very heartfelt thank you for devoting your time to the query.
While the query was raised, I was busy simulating some circuits by myself. En route, I arrived at a circuit which gives me the required oscillations. The circuit…
Hi Nidi,
You might be able to follow the function generator with a single power op amp stage. Since it is a function generator that means it puts out more than just a sine wave and will likely require much higher bandwidth than 100 kHz, and 12 Vrms…
Part Number: DRV401 Other Parts Discussed in Thread: OPA552 , DRV411 Dear Technical Support Team,
Do you have an example for external compensation coil driver?
I'd like to know what type of external amp should I select and example schematic, what…
Sorry, guys.
After reading some materials like this
https://e2e.ti.com/blogs_/archives/b/thesignal/archive/2012/05/23/why-op-amps-oscillate-an-intuitive-look-at-two-frequent-causes
I still didn't get it.
kai klaas69 said: that your scope plot…
Hi Venkatesh,
My apologies, you are correct. For a higher voltage application, I would recommend the OPA2990 or the TLV9302. Both are op-amps which can support up to 40V supply. For a higher bandwidth part, look at the OPA552.
-Paul