Hello Seema,
We have the THS3121 SOIC (D) which is pin compatible with LM7171 SOIC (D). However, the THS3121 is not as fast as the LM7171, but will have the output current ability you would need. There is also the THS3491 which is not pin compatible…
Hello Abdullah,
I just checked and it looks like a model for the TLE2301 has not been underway. The model development responsibility has moved from our applications group to another. I do not know of any plan they have to develop a model for this legacy…
Hello Davide,
The OPA552 has a common-mode input voltage (CMV) range that extends from (V-) + 2.5 V to (V+) -2.5 V. This is the linear input voltage range. If your your V- supply is 0 volts, then the minimum CMV voltage that should be applied to the…
Thanks, Garrett.
Garrett Satterfield said: see the attached TINA files.
I cannot see your attached file. Can you re-upload them, please??
For this upload, can I request a schematic that has both DAC60504BRTET as the DAC and OPA552 as the Op Amp…
Hello David,
According to our master list of technical collateral, no SPICE model was ever created for the TLE2301. We're in the process of updating old models and creating models for parts that have none, but the TLE2301 is not currently in the queue…
I deeply appreciate your help, Thomas.
Thomas Kuehl said: Note that the load RL isn't connected to ground but is connected between the OPA454 output and the sense resistor which connects to ground.
Thomas Kuehl said: That may not be usable in your…
Hello Nicola,
I would use something similar to https://www.ti.com/tool/TIPD184 . I have attempted that and another option in the lab. This could be a lot of power depending on your configuration so make sure all the required heat sink are done to meet…
Duke of DACs,
I am driving my DAC8806 with an FPGA at 3.3v. Last week a GPIO pin on the FPGA quit working. It is connected directly to pin28(reset) on the DAC8806. I thought nothing of it as the FPGA has gone through a year of testing. I replaced the…
Part Number: DAC8806 I am driving my DAC8806 with an FPGA at 3.3v. Last week a GPIO pin on the FPGA quit working. It is connected directly to pin28(reset) on the DAC8806 . I thought nothing of it as the FPGA has gone through a year of testing. I replaced…
Hi Chen Jiao,
The best replacement for the LHV870 seems to be the LME49860 and it comes in a 8 pin SOIC package. Is that pin-to-pin for the package you are currently using?
As far as replacing the LM6588, I would look at these:
LMV881
OPA551,…