Part Number: OPA567 Hi team,
Do we have EVM for OPA567? Customer want to evaluate the performance using the EVM. Could you help check?
Thanks and Best Regards,
Will
Part Number: OPA567 Is there a limit to the value of ILIM resistor that can be used for OPA567? I'm looking to limit it to ~150 mA yielding an ~77k ILIM resistor. Any issue with that?
Part Number: OPA567 Dear TI support team,
I am looking for a voltage amplifier with the following specifications:
input voltage = 3.3 to 5 V,
output voltage = upto 1000 V,
frequency = 20 to 30 kHz
current = 5 to 10 mA.
Kindly suggest a suitable prod…
Part Number: OPA567 Other Parts Discussed in Thread: OPA569 Hi support,
My customer is very concern about the longevity for this product, as we can see the datasheet is generated in SEPTEMBER 2005. Is this part plan for EOL? is it still recommended for…
Part Number: OPA567 Hi,
Im planning on using the OPA567 in a battery simulator circuit. One concern I had is how the circuit behaves with large load capacitances (1mF bulk cap). I simulated it in TINA and the stability looked okay (1ohm Riso), but wanted…
Part Number: OPA567 Hello,
i have the following problem with the OPA567 Power-OpAmp. Here is my brigde circuit. My load is a 2.25mH 2Ohm Coil.
The OpAmp is powered with a 5V single supply. My Reference Voltage (Midvoltage) is 2.5V. 2.5V at Input corresponds…
Part Number: OPA567 Other Parts Discussed in Thread: OPA2335 , OPA335 , BQ25121A I have made a battery simulator based on OPA567 (see picture). However, the output voltage contains the high ripple voltage (see picture) when no load. I have checked voltage…
Part Number: OPA567
Hi,
I tried to make my IFLAG high after EN is high with Vin and Vset are both 2.5V but failed.
I was checking any potential cause and I found my Iset pin (pin6) is always 0V. I thought I will measure a +1.18V.
Will there really be…
Sato-san,
If you want to add a protection diode across the OPA567 supply pins a 3 Amp Schottky diode would be a good choice. The forward voltage of a Schottky diode is lower than that of the substrate diode. It will turn on at a lower voltage protecting…
Part Number: OPA567 Hi, staff
Please ask questions using the waveforms on page 9 of the OPA567 data sheet (SBOS287A).
Q1. The lower left waveform “ENABLE 10Ω Load” has a ± pulse output. After ENABLE transitions from Low to High…