Part Number: OPA569 Hi,
Datasheet of OPA569 mentions that multiple devices can be set with a "master" device and slave devices connected through 2 paralleling pins.
1) What is the maximum number of devices that could be set in parallel this…
Part Number: OPA569 Other Parts Discussed in Thread: OPA548 , , TLV4110 , TLV4111 , OPA2677 Hi Team,
Our customer is looking for a voltage follower with current sink capability of 150mA that will be driven by a single 5V supply voltage, has an input voltage…
Hi Daniel,
Sorry for delay response. As far as your latest question goes regarding "the current through T1 as the dominant noise source and as I only need to drive about 125 mA, could I get rid of the pass transistor T1 and drive the laser diode directly…
Part Number: OPA569 Is the ThetaJC measured to the bottom or top of the IC package on the OPA569? It has a thermal pad and low thermal resistance of 0.37*C/W, so I wanted to make sure the location was correct for heatsink purposes.
Part Number: OPA569 Hello,
I'm using the OPA569 as part of a TEC driver. One side of the TEC is OPA569, other is an half-bridge. The driver can both heat or cool, switching the current direction, using the half bridge.
The amplifier is in unity gain…
Part Number: OPA569 Hi, TI Expert:
I have a question about OPA569, about the sink current or sink power capability?
OPA569 can output 2A current, I can undertand it as source current capability, then what's the sink current, the same as output current…
Part Number: OPA569 will use 3x OPA569(6A) in 6A Battery application.
here are some questions below:
1)Can Imonitor (pin19) parallel tie together for 6A Max current application.?
2) is there any description about equation IM=ITEC/475 in figure20 of datasheet…