Part Number: OPA604 Other Parts Discussed in Thread: OPA827 Tool/software: Hello,
first of all sorry for the part number inconvenience but choosing OPA606 is not possible in the menu so i did choose 604.
We did use OPA606KP and KM for our amplifiers…
Part Number: OPA604 Hi Team,
As per OPA604 datasheet, Absolute maximum rating for Power Supply Voltage is ±25V.
Is it possible to use this op-amp by connecting Vs+=40V and Vs-=0.
Regards,
D.Meenalochini.
Part Number: OPA604 Hi Team,
We were planning to use OPA604AU op-amp with Ground referenced V+ (40V ) supply.
Can you please suggest me How to handle Offset trim pins of this Op-amp.
Regards,
D.Meenalochini.
Part Number: OPA604 We have a batch (92AE7) of OPA604AU devices that fail to meet their specifications in terms of slew rate and settling time when used as a voltage follower on +/-15V rails. The parts were sourced from a franchised dealer.
The example…
Part Number: OPA604 hi,
i am working the below attached circuit for my input voltage range of 9mV to 14mV so that i can get the output from 0 to 2.7V . i am feeding 10mV at the input,the output is oscillating from .5 to 1V which i have observed in scope…
DC offset is tested in production so unless the part is damaged (check another unit) or oscillates ( check the output for stability with a scope ), it must be within the max limit.
If the part does not osciallate or is damaged, please confirm the value…
Part Number: OPA604 Hi
The absolute maximum voltage rating for the opa604 is +/-25VDC. We are powering the part at +/-24VDC. We need to replace an obsolete DC-DC and the new part shows some overshoot when power is applied so that the voltage rises to…
Kuramochi-san, Did the information I provided resolve your OPA2604 voltage follower peaking questions? If so, please close this E2E inquiry. Regards, Thomas Precision Amplifiers Applications Engineering
Other Parts Discussed in Thread: OPA2604 , OPA604 We are currently using the OPA2604 and are concerned about the Supply Voltage spec being limited to +/-20V and the 26 week lead time. We are considering changing two of the OPA604 and I would like to know…
Other Parts Discussed in Thread: OPA604 Dear All,
Let me ask about setting of Pin of OPA604. When a user does not use the Offset Voltage Trim function, may the user make Pin#1 and Pin#5 Open?
Pin#1: Offset Trim Pin Pin#5: Offset Trim Pin
Best Regards…