Part Number: OPA627 Other Parts Discussed in Thread: OPA1656 , OPA1642 I am in the process of restoring and upgrading several pieces of the vintage Kenwood Basic C2 preamplifier. it has 4 op-amps as follows:
1 - NJM4580D mounted in the phono preamp Section…
Part Number: OPA627 Hi experts,
My customer used CAN package of OPA627 and SOIC package of OPA627.
However CAN package has a bit more noisy than SOIC package. How should you consider the difference in noise between CAN and SOIC packages? It would be helpful…
Part Number: OPA627
Hi,
in the related post, Art Kay gives the method of calculating R1 noise and Rf noise independently.
But I find that it doesn't count for BWn.
I wonder how to calculate BWn for R1 noise and Rf noise.
For example, I think Rf noise…
Part Number: OPA627 please tell me how to download the hand-build model (Tina) which shows in TI Precision Labs Op amps Video /Noise/Verifying the noise model. ( Op amps | TI.com )
since, the resource link ( Download the TINA-TI Spice Models for our video …
Hi Nasifa,
This approach will not work for your EXT node because you are removing the feedback component of the loop. The output is modified by itself through feedback so by removing the feedback you are fundamentally changing the output signal.
This…
Part Number: OPA627
Hi,
In TI Precision Lab Training about OP AMP noise part3,
voltage noise is divided into 1/f noise and broadband noise.
1/f noise is calculated with a complex equation.
Can we use the parameter offered in the datasheet "input voltage…
Part Number: OPA828 Other Parts Discussed in Thread: OPA627 , OPA140 , OPA2828 , OPA827 Hello,
We have legacy TIA for photodiode that was using OPA627. TI lists OPA828 as being a "drop-in" replacement for it however after just swapping OPA627 to OPA828 device…
Part Number: OPA627 Other Parts Discussed in Thread: OP07 Hi,
1. the data is as below, why?
the Input voltage noise density at 1kHz input voltage noise
OPA627 5.2nV/sqrt(Hz) 0.6uV
OP07 9.8nV/sqrt(Hz) …
Part Number: OPA627-DIE Other Parts Discussed in Thread: OPA627 What is the correct operational temperature for the OPA627-DIE?
On your webpage it states that the device is a "high temperature" device, but the specification states "25 to 25".…
Part Number: OPA627 Dear Support,
KIndly help me on the part number OPA627BP (DC:1931+, COO: Malaysia)
Based on X ray, found wire bonding and lead frame design is different. Kindly help to check and confirm if this is valid and normal.
Please refer to…