Hi Vindhyachal
Please take a look at Figure 2 of the ADS804 datasheet. I think that combination including the OPA691 is very close to what you are looking for. The CMOS output drivers of the ADS804 can operate with 5V or 3V I/O supply.
Best regards,
…
Other Parts Discussed in Thread: OPA171 , OPA691 Is there any listing available of Altium compatible PSPICE simulation models for TI parts?
I know that the standard application package for the former National Application engineers was Altium so I expect…
Other Parts Discussed in Thread: THS3091 , OPA691 , OPA690 , OPA2674 , OPA2673 hello i want high speed high current op amp for 10MHZ function generator which i developing and can match to 50R output thanks
You are correct, but since these groups are always doing devices for the next rounds of test equipment they always have to do better than anything you can buy. In HD work, source cancellation methods are normally used, one of the very few published references…
Other Parts Discussed in Thread: OPA695 , OPA684 , OPA4872 , THS3092 , THS3091 , THS3201 , THS3202 , OPA694 , OPA691 Hi,
I'm a total newbie to choosing amplifiers and i need an operational amplifier to amplify a sine signal from 1Vpp to 10 Vpp (Gain=10) at a frequency…
Other Parts Discussed in Thread: VCA824 , OPA691 , OPA693 , LMH6502 , LMH6503 , LMH6504 , LMH6702 , LMH6703
Hello.
We have a system running at a fixed 175MHz. The VCA824
variable gain amp is used for Amplitude Modulation, the output voltage varies
between…
A gain of 1 to 10 is a large range for a voltage feedback (VFB) amplifier so a current feedback (CFB) is probably the best fit, so I would suggest considering the OPA694, OPA695 or OPA691. Current feedback amplifiers are not restricted by gain-bandwidth…