Part Number: THS7376 Other Parts Discussed in Thread: OPA361 , OPA360 , OPA692 Hi team,
Do we have suitable device to replace SN1603? Thanks.
https://datasheet.lcsc.com/lcsc/2107141543_3PEAK-SN1603-TR_C155438.pdf
Other Parts Discussed in Thread: OPA692 , OPA355 , OPA357 , OPA358 , OPA361 , OPA360 , OPA362 , TL592B , UA733 , LMH6570 https://www.rohm.com/products/audio-video/video-amplifiers/isolation-amplifiers/bh7673g-product
Hi Teams,
I would like to searching for HD-TVI…
Thanks for detail, makes sense, add the output DC offset range to your desired output Vpp and see if you might be clipping into the supplies.
The THS4304 does not have an internal feedback (parts like the OPA692 do, but do not operate will on 3.3V supply…
Other Parts Discussed in Thread: OPA692 Hi,
I'm using OPA692 as a buffer for my analog video signal which then goes into an adc. I read the datasheet but cannot get a clear idea of the maximum output voltage that the chip can produce @ 5V power supply…
Hi Neelam,
I would suggest using the OPA692 instead of OPA693 or THS7314 for driving more than two video lines. The linear output current drive for the OPA693 or THS7314 is limited to drive only two video lines, whereas the OPA692 would be ideal for…
Other Parts Discussed in Thread: OPA693 , OPA692 , LMH6704 Hello,
Our customer are searching for tri-level sync signal driver.
The video signal is SMPTE 240M spec.
Could you recommend a good amplifier?
The customer want the amplifier with 6dB fixed gain…