Part Number: OPA828 Hi,
I’m working on a TIA design using the OPA828 op-amp.
The TIA input is connected to an axial wire soldered to a metal pin, which I then enclosed with heat-shrink tubing. I used a lighter to shrink the tubing.
After doing…
Part Number: OPA828 Other Parts Discussed in Thread: OPA192 , OPA145 hi Sir
old desin use the ADA4627-1ARZ, we use the TI/OPA828 to replacae ADI solution
but, not complete to replace it, due to we need the trim pin to adjust the offset
i know…
Part Number: OPA828 Other Parts Discussed in Thread: OPA2210 , DUAL-DIYAMP-EVM Hi
can I get DIYAMP-SOIC-EVM and DUAL-DIYAMP-EVM gerber file for opa828 & opa2210 for TIA application?
Arrvie
Part Number: OPA828 Tool/software: When operating with +15v and gnd as the supplies to the op-amp, how close to zero volts can the output drive? (load < 1mA) ?
Does operating close to the negative rail (ground) reduce the op-amp precision (drift, offset…
Part Number: OPA828 Tool/software: Hello,
I'm working on a TIA circuit to detect 100pA current, and bandwidth need to be around 15kHz. The current is generated by a voltage buffer on the PCB and a 10G resistor connected by coaxial wire.
And I found…
Part Number: OPA828 Kind of scanning through the OPA828 datasheet (2022 update) this plot
So that Aol over temp plot should say 1/Aol and I really doubt it flips polarity over temp
Part Number: OPA828 Other Parts Discussed in Thread: OPA320 , OPA328 , OPA3S328
Tool/software:
Hello,
I find my TIA output is not correct.
And when I remove the input (so nothing connect to RF1), the output should be near zero. But one of my boards…
Part Number: OPA828 Other Parts Discussed in Thread: OPA192 , Tool/software: Hello team,
My customer is evaluating OPA828. The electrostatic discharge of OP828 is ±2000V. But some opamp (ex OPA192) cases are ±4000V.
Is this due to the difference…
Part Number: OPA828 Tool/software: Hi,
I am simulating Howland charge pump with OPA828. I see the edges are getting chipped off in my output. Any idea on why this could happen?
Thanks,
The input rise time is 10uS and 5V at 100Hz.
Part Number: OPA828 Other Parts Discussed in Thread: OPA827 , Tool/software: I'm using the OPA828 as a preamp for a reproduce head in an analog magnetic tape recorder. This is the first time I've tried using a FET-input opamp for this job, because opamps…