Well it is difficult to comment for all parts across the different groups and timeframes in which they were done -
For specs like the input bias current on the OPA837 for instance, that is just the mean it is unipolar - I am often suspicious of +/-…
Part Number: OPA365 Other Parts Discussed in Thread: OPA727 , OPA863A , OPA835 , OPA837 Hello,
I’m looking for a precision op-amp recommendation that can be used as an error amplifier (supply = 12 V nominal) and whose output becomes high-impedance …
Part Number: ADC3644 Other Parts Discussed in Thread: OPA837 , , REF3318 Hi team,
In the EVM of ADC3644, 1.6V of VREF is divided and supplied by REF3318 and OPA837. Is this because there was no 1.6V reference? If I use the ADC3644 with an external reference…
Part Number: OPA817 Other Parts Discussed in Thread: THS4541 , OPA837 Tool/software: Hello TI experts, my design includes two OPA817 with a gain of 1.1 and 3.3. Are there some recommandation from TI for the "best" feedback resistor values in case of …
Part Number: OPA838 Other Parts Discussed in Thread: OPA847 , OPA2626 , OPA625 , OPA350 , OPA626 , OPA837 , OPA810 Tool/software: Hello
When I perform simulation of OPA838
The result is stable
But when I add a feedback capacitor, the circuit…
Hi Benham,
The OPA837 is the best match for your system requirements as many of our transimpedance amplifiers have much higher power consumption than the OPA837/OPA838. The OPA837 is also unity gain stable. The OPA837 however, does have a larger voltage…
Part Number: OPA836 Other Parts Discussed in Thread: OPA838 , , OPA837 Hi team,
My customer is using our OPA836 & OPA838 now.
And they wonder if we have a newer device to recommend.
Requirements:
BW: >200MHz
slew rate:>200V/us
Iq:<1mA
…
Part Number: OPA838 Other Parts Discussed in Thread: OPA855
As all the datasheet has mentioned, we need to remove GND and PWR plane underneath the negative inverting pin and the output pin of the operational amplifier (It is important to avoid ground…
Part Number: LMP7704-SP Other Parts Discussed in Thread: LMP7704 , , OPA837 Hello,
I am looking for the TINA model file that is presented in SNOAA75A (Space-Grade, 100-krad, 125-kHz Photodiode TIA Circuit),
A snippit from the pdf is shown below. …
Other Parts Discussed in Thread: OPA837 Hi engineers, for deepen understanding of op amp parameters, I want to build different test circuits for various op amp parameters, but the datasheet just introduce some test condition, so I need some document which…