Part Number: OPA860 Tool/software: Hello,
Could someone explain why the unit on the y-axis might be incorrect? If it's not incorrect, what does the "mA/V" in parentheses next to the line mean?
Thanks,
Part Number: OPA860 Hi Kailyn & Kai,
I am practicing with the OPA860 peak detection circuit that Kailyn post.
e2e.ti.com/.../opa860-opa860-sample-hold-circuit
The circuit is consist of two-stage of OPA860. T he first for a fast rise time and the second…
Part Number: OPA860 Other Parts Discussed in Thread: OPA356 Hi team,
The customer drew the physical board according to the original post, but the actual results of the physical test were still similar to the simulation. Referenced this post:
https://e2e…
Part Number: OPA860
Hi team,
One of our customer's issues, could you please provide some troubleshooting suggestions:
I used the opa860 chip as a peak holding circuit, with an input of a 10ns pulse signal. I saw a similar post on the forum and simulated…
Part Number: OPA860 Other Parts Discussed in Thread: OPA861 Hello,
I designed a peak hold circuit using OPA860 and OPA861, a transistor amplifier chip, where the physical design and simulation design principles are similar. However, without its built…
Part Number: OPA860 Hi team,
One of our customer's issues, could you please provide some troubleshooting suggestions
The customer made a circuit board based on the circuit in the post below (from Kai) and after testing found that the output was around…
Hello Sean,
I bought, received and assembled OPA860 EVM DEM-OTA-SO-1A. Components that I installed are as following:
power: +-5V, 10uF and 0.1uF at both voltages
OPA860 is from the same batch as previous parts used
OTA section: RB2=51, RB1=150, RE=150…
Part Number: OPA860 Other Parts Discussed in Thread: OPA861 , OPA615 , LM13700 , OPA2210 Hi Team,
The customer is working on a voltage-controlled current source and would like to use an operational transconductance amplifier (OTA) integrated circuit and they…
Part Number: OPA860 Hi. We want to use OPA860 as a current feedback amplifier in one of our designs. As such, we need to prepare an FMEA. I have one failure that I am struggling with. "What will be the effect on the signal path if the current setting…
Hello Hale,
The OPA1S2384 remains an option for your customer. I also have seen prior support on projects for sample & hold with the OPA860 and OPA615:
OPA860: OPA860 sample& hold circuit - Amplifiers forum - Amplifiers - TI E2E support forums…