Other Parts Discussed in Thread: PGA206 , PGA280 Hi,
we are using PGA206 on a analog electronic board since 15 years, and we are regard to redesign a new one.
Do you new parts with same quality of PGA206 (Vin up +- 12v) and with a SPI interface ?…
Part Number: PGA281 Other Parts Discussed in Thread: PGA280 , PGA206 , INA851 HI TI,
Since PGA281 is out of stock now, it is necessary to find an alternative.
Is there any recommended circuit scheme using operational amplifier or instrument amplifier…
Part Number: PGA281 Other Parts Discussed in Thread: PGA280 , PGA206 , INA851 My circuit function is to measure 0-7.4A current. Pga281 is used for current sampling, and the accuracy shall not be higher than 500uA. Since pga281 is out of stock, I hope…
Part Number: PGA281 Other Parts Discussed in Thread: THP210 , PGA206 , PGA207 Is there a product like PGA281 that can accept input signals of130Khz as well?
We need a high-precision instrumentation amplifier, for very low input signals.
The secondary…
HI Rekha,
Attached is a list of precision programmable gain amplifiers that can support outputs up to +/-10V.
As Kai has mentioned, it would be useful to know the DAC that is used on this application, as well as the input amplitude and frequency/settling…
Other Parts Discussed in Thread: PGA281 , PGA206 In an application case where only the IN-P is used for 0-5 Vdc input, and correspondingly only use VO-P, when VOCM is tied to VSON, can the PGA281 be used? I realize that the VO-N will saturate low and…
Hi Shivakant,
I don't think ISO124 will meet your specifications, as its input noise is 4uV/rtHz, and it has a ±50mV max offset spec - 2x your minimum input signal range.
The closest our PGAs get to a sub-10nV/rtHz noise level would be PGA203, PGA205…