Part Number: PGA2320 Dear All,
I designed a new Audio Pre-amplifier PCB board in which I use PGA2320 in order to control the volume by a Microcontroller. To test the sound performance, after analyzing the THD+N, frequency response, Slew rate etc ..…
Part Number: PGA2320 Other Parts Discussed in Thread: PGA2310 Hi team,
Does TI have EVM for PGA2320?
Is it available for supporting new customer design?
Regards,
Itoh
Part Number: PGA2320 Other Parts Discussed in Thread: OPA325 , OPA1688 Hi Team, We want to use a speaker in one of our products. The system is battery-operated (3.7V nominal voltage). I will need an audio input circuit to digitize the audio signals. I…
Part Number: PGA2320 Other Parts Discussed in Thread: PGA2311 , The PGA 2320 Dec 2004, data sheet provides no detail on how/when the 16-bit serial register contents are transferred to the gain switch 'holding register' under basic operating conditions…
Part Number: PGA2311 Other Parts Discussed in Thread: PGA2310 , , PGA2320 Hi TI experts,
We are looking for volume control IC.
Do you have S/N spec of PGA2310, PGA2311 and PGA2320?
(Test condition : Vol=0dB,Rg=0 Ω, A-weight)
Please check it. …
Part Number: PGA2320 Other Parts Discussed in Thread: UCC21750 Hello Team,
My Customer is looking for the complete thermal data for the PGA2320IDW. Checking with the datasheet this is data is not included. Can you share with us the thermal data of this…
Part Number: PGA2320 Other Parts Discussed in Thread: LT1054 Hello,
I just would like to know if it's possible to supply analog part of PGA2320 with a 30VDC single voltage instead of +/-15VDC ?
Of course digital part will be supply with something…
Part Number: PGA2320 Hello Guys,
Good day. One of our customer is looking for the input impedance (minimum) itself of the PGA2320 because the once specified on the datasheet is the source impedance of the previous stage which should be less than 600ohms…
Simon Quarry1 said:
I'm afraid that does not answer my question.
I need to know the minimum input impedance of the PGA23xx.
RTFDS: for PGA2320, see Page 3, "Electrical Characteristics," under parameter "DC Characteristics," it's right there…