Hi Mohammad,
The PGA308EVM uses a windows-default HID driver and shouldn't need any additional drivers installed. The EVM should show up in Device Manager as "HID-compliant vendor-defined device" with a VID of 0x0451 and a PID of 0x2F90, 0x2F91, 0x2F92…
Part Number: PGA308 Hi Team,
The customer is using PGA308 for his design. He writes a PC software to configure the registers. And he uses his board. When the customer writes the configuration data into the registers of PGA308, the PC software shows…
Hello ZhenGuo,
1) Can you please verify all jumpers on the PGA308EVM and the USB DAQ board are in the correct position. Specifically, please verify/confirm on the USB DAQ board that JUMP3 is in the EE_ON position as shown on the image below, with the…
Hello KoT,
Steps 1-13 document the calculations performed by the EVM software to obtain the correct calibration coefficients during the calibration routine.The PGA308EVM-USB performs the calibration routine in the software. The calculations are based…
Other Parts Discussed in Thread: PGA308 , PGA308EVM , MULTI-CAL-SYSTEM , PGA309 Hello, all
Now we have one inquiry regarding auto calibration program for PGA308 from our customer who is about to start their mass production model on which PGA308 is used…
Hi Dmitrii,
I'm looking into this but I have a couple of basic starter questions regarding your setup, as I don't want to make any assumptions.
1. Just to confirm, you are using a 5V supply when programming the device, rather than the 3.3V shown in…
Hello Vladimir,
A differential input range of ±200mV will work just fine with the PGA308. Make sure that the common-mode input range is not violated, preferably held close to mid supply.
If you would like to test the behavior of the device when calibrated…
Hello, thank you for your continuous support toward each inquiries.
We would like to know the baud rate setting on PGA308EVM, please see each items below and feedback us with your comment.
Q1. On PGA308EVM, is the baud rate setting handled automatically…
Hi Patel,
If you are interested on only testing one sensor, the PGA309EVM allows you to perform calibration of a real external sensor using the PGA309EVM-USB.
The software of the Multi-Cal system is not compatible with the PGA309EVM USB since these…
Hi Greg,
I don't see anything on a master reset response in the PGA308 documentation.
The easiest way for you to debug your communication is probably to compare your 1W transmissions to that of the PGA308EVM. If you send me your shipping address…