Part Number: PGA460 Other Parts Discussed in Thread: SN65HVDA100-Q1 , TLIN1029-Q1 , I want to connect several PGA460 through LIN。
My PGA460 Power VPWR=7.8V,
But Master LIN is12V, Can I connect PGA460 IO pin to Master LIN directly?
Thanks
Part Number: PGA460 Other Parts Discussed in Thread: TIDA-060024 , , Hi Team,
Our customer uses a formula of “ Jaju747 ” and “slaa732a” to calculate "CTUNE ".
However, typical values for tuning capacitance ranges is different.
- Jaju747 / 2.2…
Hi Brandon,
thanks for the response. I will attach the most important instructions we are working with: Triangulation.pdf pga460.pdf .
We have already attached the PGA460 to a MSP-EXP430F5529LP board. Do I get your point correct, we need to connect…
Part Number: TDC1000-Q1 Other Parts Discussed in Thread: TDC1000 , TUSS4470 , PGA460 Hello,
I am considering TDC1000-Q1 in our my new product development.
Referring to chapter 11 of TDC1000-Q1 datasheet, I see the recommendation is for 4 layer PCB…
Hi Jack,
Thank you for conducting the board swap, this seems to confirm it is an issue with the TI-GER board.
It may be possible to debug the issue in the TI-GER board, but TI does not have any published documentation for the TI-GER hardware. If possible…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460 Hi,
our company uses PGA450Q1 connected to a waterproof transducer.
this gives us measuring range of >~35 cm up to ~4m.
we would like to reduce minimal distance to ~3cm.
of course…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA460 We are using Push-Pull configuration for the burst mode.
How to choose the tdeadtime in the Deadtime Formula(DEADTIME = FOSC × tdeadtime)
the ON_A = 8A (based on the ON_A = dec2hex(FOSC…
Part Number: PGA460 Hi Team,
We have two questions.
---------
[Q1]
We would to know the difference between " Time Decoupling " and " Temperature Decoupling " and effectiveness.
Because, we are considering which method to use.
Could you…
Hi Matteo,
A few items to verify:
What microcontroller are you using? Is it a 3.3V or 5V logic level micro? The PGA450-Q1 is 5V only.
What voltage are you supplying the PGA450-Q1? A minimum of 7V is required, so a USB based 5V supply will not…
Other Parts Discussed in Thread: PGA450-Q1 , PGA460 , MSP-EXP430F5529LP , MSP430F5529 I am currently working on an application that requires an ultrasonic sensor to determine the ice level in an ice making machine.
I need to be able to read levels from…