Part Number: UCC28782 Other Parts Discussed in Thread: PMP23224 Hi,
I have tested PMP23224 board with an output of 8.4V, 3A it is working fine.
After that I have changed layout replaced with all the 0402 componnets with 0603 size
as well as leade…
Part Number: PMP23224 Tool/software: Hi Team,
We are in the process of constructing the PMP23224 PoC setup and require specific transformer details, including the number of turns, AWG, and other relevant specifications.
Could you please assist us…
Part Number: UCC28782 Other Parts Discussed in Thread: PMP23224 Hi all,
with respect to PMP23224 demo circuit, I would like to set CC limit at 3A only.
I have traied R63 increses upto 500 ohms. But current limit is not changing.
and also incresing…
Part Number: BQ40Z80 Other Parts Discussed in Thread: TL103WB , PMP23224 Tool/software: Hi TI,
Iwant to use a Bq40Z80 battery pack manager to realize a BMS and I have some questions:
I read an interesting AN SILA619 that use the TL103WB as CC-CV controller…
Part Number: UCC28782 Other Parts Discussed in Thread: UCC5350 , UCC27712 , LMG3622 , LMG3616 , PMP23224 Hello,
I am checking the constants input into the UCC28782 calculation tool. In order to use UCC5350SB as a gate driver, I am considering the constants…
Hi Minseong,
We currently do not have a wide input voltage, high power flyback reference design for 300W, However, we do have PMP41063 which is an example of a 300-1000VIn 48W reference design based on the UCC28730 (This is an ultra-low standby power…
Hi Vinayak,
Thank you for reaching out.
300W seems very high for flyback. We have some designs upto 220W using UCC28782 which is a ACF + ZVS flyback.
https://www.ti.com/tool/PMP23224
UCC28781 is only ZVS flyback, nevertheless it might be possible…
Joe,
No matter what LLC controller to use, the fundamental of LLC topology doesn't change. >3x output voltage range is doable but requires careful design and will need to trade off certain performances, like efficiency. You can consider add a boost…