Part Number: PMP30104 Hi Experts,
We are looking for PMP30104 but this is a design file and cannot be purchased. Are there any equivalent or similar EVMs to PMP30104 to purchase?
http://www.ti.com/tool/PMP30104
Regards,
Uchikoshi
Part Number: TPS40210 Other Parts Discussed in Thread: PMP30104 Dear all,
in the reference design, PMP30104, a multiplied sepic capacitor charger is presented. It boost 15Vin to 420V/80mA out. I need some variations (higher input voltage, higher output…
Part Number: PMP30104 Other Parts Discussed in Thread: TINA-TI , TPS40210 , , TLC272 Tool/software: TINA-TI or Spice Models Sir,
I am Trying to run the schematic in Tina, the output voltage produced is in mV is not as specified. I am attaching TSC file. …
Part Number: TLV9102 Other Parts Discussed in Thread: PMP10081 , PMP30104 , TLC272 , , TINA-TI Hi support team,
TLC272 is used in PMP10081 and PMP30104.
www.ti.com/.../PMP10081 www.ti.com/.../PMP30104
Is it possible to use TLV9102 instead of TLC272?
Regards…
Part Number: TPS40210 Other Parts Discussed in Thread: PMP10081 , PMP30104 Hi support team,
I want to trickle charge Ni-Cd battery with SEPIC. Is it possible to realize a constant current circuit with TPS40210?
Vin: 24V Vout: 30V or less Charging current…
Patrick, TI has a Reference Design area where you can search for designs.
I looked for 300Vout and DC input, per the link below.
www.ti.com/.../index.html
3 designs are presented that show the concepts needed for your requirements.
At this low current…
Part Number: TPS40210 Other Parts Discussed in Thread: PMP30104 Dear support member,
My customer think follwing sepcification.
Vin :17V~19V Vout:350V Iout:1mA fsw:500kHz
There was reference design PMP30104, could use at this specification?
www.ti.com/...…
I see PMP20212 is "close" but would certainly need some work for extra V and I: http://www.ti.com/tool/PMP20212 .
added>
also check www.ti.com/tool/PMP30104 and
Hello Getssy,
With such a high boost ratio there are typically several stages used. Boost + charge pumps, flyback with stacked windings, multipled SEPIC, are some of the topologies used. Output currents for a high boost ratio are usually in the 10's of…