Facundo,
I don't think CCS works or was tested on a 64-bit Linux, since I found several issues when trying to start it in Ubuntu 9.10 64-bit. I found a similar problem caused by incompatibilities with the GTK library and I imagine it is because Eclipse…
Other Parts Discussed in Thread: AM5728 Tool/software: Linux we need mmc3 support sd card in am5728 platform base on ti-processor-sdk-linux-am57xx-evm-03.01.00.06 ,
the patch as attachment, my question is:mmc1/mmc2 can send init cmd from controller…
Other Parts Discussed in Thread: DRA752 , PMP Hi,
Background:
We are working on the am57xx-evm with ti-processor-sdk-linux-am57xx-evm-02.00.01.07. With pre built images we are getting linux login prompt and web matrix browser. Every thing working…
I have installed EZ SDK ( ti-ezsdk_dm814x-evm_5_04_00_11_demo) and able to boot pre-built linux image(uImage) from SD card on DM814x EVM board.
My aim is to use the same uImage and try to boot it from SD card on DRA6XX Automotive Media processors REV2…
Thank you,
I've tried this out yesterday. (Changes have to be made; pragma isn't known in GNU toolchain an some other issues... now it compiles and a elf will be created.... more than less.)
Now there's the .resource_table section, but I'm not able…
Hi Ed,
Edmund Yew said: I am starting my config with this default config file included in the kernel download package: omap2plus_defconfig
Which version of the Processor SDK linux release do you use? Please use tisdk_am335x-evm_defconfig instead.…
Hi Matteo,
We would recommend to create a new project and update SDK.
However, since you are using SDk version 1_10_00_05. The SDK start from 1_xx should work for the "MSPM0L1306" silicon. So, your issue might not related to the SDK. Then I check…
Pavel,
Thanks again for the suggestions, apologize for the delay in response we were moving offices. Yes, I am editing the Linux DTS file, am437x-idk-evm.dt, in the am437x_evm_sdk/board-support/linux-4.14.79+gitAUTOINC+bde58ab01e-gbde58ab01e/arch/arm…
Hello Karan,
Any updates?
We would also share the linux logs that we observed for( Log1) successful booting(In this case we had put some delay in rtos application) and the logs where (Log2)linux crashes(Rtos application with no delay).
We could…
Other Parts Discussed in Thread: OMAP3530 Hi,
I am using OMAP3530 (X3530BCUS) at 12 Mhz, Micron NAND at GPMC CS0, SMSC9220 at GPMC CS3, Micron Memory at SDRC CS0. I require to Boot from NAND but am not able to detect the NAND Device ID. The Ethernet…