Hi Conor,
Unfortunately the PUREPATH-WL-CFG is no longer maintained, and understand how frustrating this may be.
When I have more time, I can try to familiarize myself more with this tool, though regrettably I cannot provide a timeline for this at the…
Part Number: CC3235SF Other Parts Discussed in Thread: SYSCONFIG , SYSBIOS Tool/software: #include <ti/net/utils/clock_sync.h> I define it in this way, but it still gives the following error.
void *wifiScanThread(void *arg0) { while (1) { // WifiScanAndDisplay…
Hi Conor,
Conor said: Q1. Is it possible to connect and operate TLV320AIC3263 and CC8520 via I2S, I2C, or SPI? If so, can I create a program with purepath wireless configurator?
According to datasheet, CC8520 supports:
I2S and I2C : Seamless connection and…
Part Number: CC3235SF Other Parts Discussed in Thread: SYSCONFIG , SYSBIOS Tool/software: #include <ti/net/utils/clock_sync.h> library cannot be defined in the portable project. I can define it in the network terminal code but when I define it in the…
Hello Rasty,
Please see I have attached all the patches details .
Patch 1 : To move freeRTOS libraries to MSRAM memory.
Please integrate only the change below in your linker cmd file and in my test setup I have updated linker file for different Test scenarios…
Hello George,
I tried running the command for linking through cmd using the way you mentioned as you can see in the attached screenshot, but the error still exist
txt.txt
-mcpu=cortex-r5 -flto -O0 -march=armv7-r -mfloat-abi=hard -mfpu=vfpv3…
Part Number: CC2652PSIP Other Parts Discussed in Thread: CC2650 , SYSBIOS , SYSCONFIG , CC2652RSIP Tool/software: Hello,
My project uses CC1352PSIP and it stopped working after some time. I got the following errors list of errors:
Description Resource Path…
hi bin
1、Based on linux-rt-SDK8.6.0042/mcu-sdk8.6.0018, I used ccs12.2 for uboot-gp. The following is the compilation log.
The following is the log compiled using ccs.
r5-build-log.txt
**** Build of configuration Debug for project ipc_rpmsg_echo_linux_am62x…
Part Number: MSPM0L1105 Other Parts Discussed in Thread: MSPM0L1306 , Dear Ti team,
1157.adc12_sequence_conversion_LP_MSPM0L1306_nortos_ticlang.zip
This is the souce code we modified based on adc12_sequence_coversion example, and it can build successfully…