Part Number: RC4580 Tool/software: Hello E2E experts,
I recently bought several ICs from different stores. I would like to know if both variants are genuine or if any are fake?
Best regards.
Part Number: RC4580 Hi,
We are using the TI operational amplifier RC4580IDR in our product.
As shown in the attached circuit diagram, there is a situation where the op amp’s supply pins (+V, –V) are left floating (no power applied), while an external…
Part Number: OPA1642-Q1 Other Parts Discussed in Thread: RC4580-Q1 , Dear , Audio op-amps suport Team. Is there no datasheet showing the 10Hz to 20kHz bandwidth for Maximum Output Voltage vs. Frequency in the electrical characteristics graphs for the…
Part Number: RC4580 Tool/software: Hi, Staff
The RC4580 datasheet (SLOS412D) states on page4, 6.3 Recommended Operating Conditions: TA: -40(MIN), +125(MAX).
However, the same datasheet also states under PACKAGING INFORMATION that Op Temp(℃) is -40…
Part Number: RC4580 Hi all
My customer is using the
RC4580 Dual, 32-V, 12-MHz, low noise (6.5-nV/√Hz) operational amplifier RC4580IDR
And they have this question:
The supply is +/-15V, where the -15V is delayed for power on and off vs. the +15V…
Part Number: LMV321 Other Parts Discussed in Thread: RC4580 , , LM321LV Tool/software: Hi team,
I'd like to double check with you one thing here.
Could you kindly check if we can use RC4580 on current sensing application instead of LMV321? It seems…
Part Number: RC4580-Q1 Dear team,
Can we know the ABS_max rate of Tj (junstion temperature)?
I could not find it in the datasheet. Is it same as Ta_absmax=-40 to 125C?
Thank you, Yuto Kitamura
Part Number: RC4580 Dears:
when use RC4580 in sensing project, we calibrate it in the product line, but end customer found abnormal accuracy error after several weeks work. Could you please help provide VOS VS time curve to help identify the issue?…