Hi Garrett Satterfield,
Sorry for Replay. I Planned to work with DAC8670 in QFN package. I attached Schematic for QFN package as followed in Development Board.
Please Check the Schematic to get IOUT output.
From last Baord,
DVDD-EN not connect…
Hi,
Hope you are having a great evening.
1. The datasheet update was done in May 2015 (9 months ago - not 4 years). Attached are the two versions. Version B (Revised 2012 - still include App information). Version C (Revised May 2015 Current version…
Here is a link to a document for bq20z70 and bq20z90, it has a description of the production flow in section 22. /cfs-file/__key/communityserver-discussions-components-files/196/0714.1072.slua404_5B00_1_5D005F00_application-book-for-the-bq20z70-and-bq20z90…
James,
It takes a few minutes for the voltage measurements to update capacity. You also need to calibrate the pack. I attached the general applications book for gas gauges. You can reference Chapter 22 for a detailed production procedure. They calibrated…
1. Most of the orders do come from pack manufacturers, but there are plenty of end system manufacturers that use these devices as well.
2. Yes, you will need to get access to the cells to use the bq20z45 gauge. You may be able to divide down the full…
Yes, the PRO screen is where the commands can be written and read. Your next step after setting up data flash and calibration is to start the learning cycle process. To do that, you need to enable the Impedance Track algorithm. This turns on the FETs…