Part Number: REF30 Tool/software: Hi team,
The customer find the typo in datasheet .
The max output voltage of REF3030 is not "3.06" but "3.006", right ?
They are also requesting to revise the datasheet correctly.
Regards,
Morita
Part Number: REF3030 Hello team,
I am confused about the bypass capacitor for this device.
On datasheet 9.1 Application Information, it says REF30xx doesn't need output cap, and showing 0.47uF input cap. However, on Layout Guidelines, it says to put…
Part Number: REF3030 Other Parts Discussed in Thread: REF3330 , REF3130 Tool/software: HI,
what are the dropout voltage with load current for REF30XX for full temperature range? is the maximum dropout voltage is 300mV for all REF30XX for full temperature…
Part Number: REF3030 Other Parts Discussed in Thread: REF35 , REF4132 , REF3130 Hi
How to calculate the upper and lower limit of output voltage including temperature drift? I am thinking as below, is it correct?
Regards.
Part Number: OPA357 Other Parts Discussed in Thread: TLV9101 , OPA310
Hello,
I'm using an OPA357AIDBVR (IC18) to buffer a REF3030 chip. Below I show all the circuits that have interface with the AVREF: The problem: the AVREF should follow the positive…