Part Number: REF30 Hello,
I'm having problems with the voltage reference IC. The IC is connected to the amplifier's reference pin and powered at 5V as per the schematic.
I tested the IC outside the circuit and it works, but when I put it in the circuit…
Part Number: REF30 Tool/software: Hi team,
The customer find the typo in datasheet .
The max output voltage of REF3030 is not "3.06" but "3.006", right ?
They are also requesting to revise the datasheet correctly.
Regards,
Morita
Part Number: REF30 Other Parts Discussed in Thread: REF33 , Tool/software: Hi expert,
If the REF33 input current is continuously ~36mA (>datasheet recommending 25mA load current), or even higher current to damage the device, whether it will output 0…
Part Number: REF3040 Other Parts Discussed in Thread: REF30 , REF33 , REF35 Hi,
I'm implementing an application that requires running the MCU only on battery power in the event of a power outage (expected consumption around 25uA). The request is to…
Part Number: REF33 Other Parts Discussed in Thread: REF30 , REF30E Hello
I would like to perform a noise simulation for REF3330. When I use a DC source, the result is
But if I use a AC source, the result is different.
The result is quite different…
Part Number: LM4040 Other Parts Discussed in Thread: REF30E Tool/software: I would like to know whether the shunt could work under 125℃.
Does the TCR keep the same?
Thanks!
Part Number: REF3112 Other Parts Discussed in Thread: REF30E , REF31 , REF31-Q1
We wish to verify whether there are any issues with the circuit diagram.
Part Number: INA240 Other Parts Discussed in Thread: REF30E
Hello everyone, I am designing a 48V three-phase inverter that will be connected to a BLDC motor controlled using an FOC algorithm at 40kHz.
In fact, the inverter I am designing can be connected…
Part Number: REF35 Other Parts Discussed in Thread: LM4121 , , REF30E Hello guys,
One of my customers uses LM4121AIM5-1.2/NOPB(Vo=1.250V) for thier mass-production.
They are looking for a alternative device for LM4121AIM5-1.2/NOPB because LM4121 is…
The below is taken from the REF30 voltage reference, and subnote 2 mentions that the box method is used to determine over temperature drift. This should be the common standard for all temperature drift specs for any electronic device or component.