Part Number: REF34-Q1 Hi team,
My customer asked maximum Turnon time with below condition.
- Vin=5V
- Cout = 0.1uF
Could you provide required information?
Best regards,
Nobuo
Part Number: REF34-Q1 Hi team,
My customer wants to use REF3425-Q1 with Vin=5V and Vout=2.5V condition.
From system point of view, there might be the case where Vout > Vin.
Question):
In this case, do we have internal clamp diode to stand with…
Part Number: REF34-Q1 Other Parts Discussed in Thread: REF34 Hi Team,
My customer is asking question about long term stability of REF34-Q1.
In REF34-Q1, it is described long term stability as 25ppm@1000hr, but other suppliers device shows its spec…
Part Number: REF34-Q1 Hello Team,
I'm Yuta Kurimoto TIJ FAE.
I got some question from customer about the hysteresis of Enable pin threshold. The part number is REF3450QDBVRQ1.
Q. How much thermal hysteresis the ENABLE pin threshold has? Typical…
Part Number: REF34-Q1 Other Parts Discussed in Thread: TINA-TI Hello Team,
I performed TINA-TI simulation for REF3450-Q1.
Q. As we can see in the waveform, when the Vin increase gradually, the Vout start increasing from @Vin=5V. Is this behavior correct…
Part Number: REF3450 Other Parts Discussed in Thread: REF34-Q1 Tool/software: I am using REF3450 for an automotive application. I have a question if the input voltage goes below 5V, what would happen to the output voltage.
Part Number: TMS320F28P650DK Other Parts Discussed in Thread: OPA328 , REF34-Q1 , OPA388-Q1 Hi,
I plan to configure the external reference voltage circuit as follows to drive the on-chip ADC module of the F28P650DK9 MCU in 12-bit or 16-bit mode.
…
Hello Yenwu,
You could consider REF3450QDBVRQ1, which has a recommended max input voltage of 12V.
The absolute maximum ratings list the operating temperature range as -55°C to 150°C. As long as you stay within that range, there should be no permanent…
Hi Zhang
We have REF34-Q1 in DGK package. However it is not P2P with REF50.
Can you please comment on the existing solution from competition ?
Regards
Trailokya
Part Number: REF4132 Other Parts Discussed in Thread: REF3433 , REF34 Tool/software: Hello,
looking for a 3,3 V reference voltage, I compared the datasheets of REF34xx , REF34-Q1 and REF4132 . I noticed that most of the performance figures are identical…