Hi Takahasi-san,
Apologies for the delay. So the TI-EVB has the spur at ~4.98GHz and your board has a oscillation at 3.1GHz if I understand you correctly. Is the layout of your board considerably different? Is it possible to share your board files with…
Hi,
So, 300 kHz HPF cutoff is the dominant driver. Low HPF cutoff frequencies inherently require longer ADC settling, and HPF fast initialization exists specifically to reduce that settling time 1 . Also, 11.25 MHz/µs slope compounds it: higher chirp…
Linus,
To setup the channel sounding demo you can follow the Channel Sounding Documentation .
I am not sure what you are setting up. The car node project must've been customized to automatically output the RSSI for each connection event. Additionally…
Hello Samhitha,
Samhitha Bobba said: I am still not clear with the usecase. Let's say a moving target is detected at a range x in frame n and in the next frame, you set the Rx gain with respect to previous frame's estimate. As it is a moving target…
HI, there:
I can see the picture now.
1. In the 2D FFT amplitude profile, why there has 3 colored line?
Mmwave studio postProc does not understand the TDM or BPM mode. They assume all the chirps are the same. That is why it has two main lines. The…
Hello Charles,
Regarding your first question, if you do not need open-wire detection for the thermocouple, then biasing to mid-supply on the negative lead will eliminate any possible IR losses in the thermocouple wire due to the bias resistors.
1…
Hi, Simran
nice to meet you in here and big thanks for your supporting!
my customer design an RF transmitter for MRI system. they want TI propose a digital or analog pre-distortion circuit to linearity RF power amplifier. do you have an good idea…
Part Number: AWR1843BOOST Other Parts Discussed in Thread: AWR1843 hi,
I used the awr1843boost to detect objects' range and angle, studied the Radar RF front end and processing the radar adcdata with matlab. but it seems always there is Strong reflection…
Hi Lina,
Please find my answers inline.
Lina Kim said: 1. ADC Full-Scale Input Voltage
What is the full-scale input voltage of the radar ADC?
Is it specified as Vpeak or Vpp ?
Is it referenced to a differential or single-ended basis…
Hi Ashot,
Apologies for the delay in response, I have been OoO.
While I am sad to hear that you have decided to move away from the CC3220S for this project, I'm happy to continue to provide any information I can.
Ashot Andrieiev said: If possible…