Hi Ankit, thanks — we implemented the idlePowerMode-driven approach you suggested, and it's worth reporting back because it half-works in an informative way.
What we did (per reply 2): instead of leaving the BSS free-running, we shrank the frameCfg…
Part Number: AWR2E44PEVM Tool/software: Hi expert,
We're using gPTP for time synchronization and performing time-division based sweeping with five radars to avoid mutual interference.
However, we are encountering an issue where the actual RF sensor…
Part Number: AWR2243 We are using the MMWCAS-RF-EVM (4x AWR2243 cascade, 12-TX TDM-MIMO) together with the MMWCAS-DSP-EVM (TDA2x).
Goal: stream the full raw ADC data of every frame off the board for back-end processing on a host. Current frame configuration…
Hi Raymond,
We are considering using the TL5580A in a single-supply configuration with a +5V power supply. In this case, what would be a reasonable estimate for the valid common-mode input voltage range (Vicm)?
We understand that the width of the…
Part Number: TAS2505A-Q1
Hi TI Team, I am using the TAS2505A-Q1 in an automotive telematics application.
For power-tree analysis, I need the active current consumption for each supply rail:
SPKVDD = 3.3 V
AVDD = 1.8 V
DVDD = 1.8 V
IOVDD…
Part Number: IWRL6432AOP Hi,
We are designing the new mmWave module based on L6432AOP.
According to the statement on page 33 of the attached document "Parameter Tuning and Customization Guide for the xWRLx432 Motion/Presence Detection Demo," For tracking…
Part Number: DDS39RFS10
hello,
We want to support output frequencies of 50KHz to 1000MHz.
So, an external RF choke (inductor) is not a feasible solution.
If I use an external PU resistor, I can support this frequency range easily.
See below…
Part Number: CC2650MODA Tool/software: Hi TI expert,
As email title, is there 3D plot of CC2650MODA for customer to do mechanical and placement estimation?
Meanwhile, is there RF clear zone SPEC requirement for it?
Sincerely.
Part Number: AWR2E44PEVM Hi Team,
I am working with the AWR2E44PEVM and require assistance in generating a specific configuration file (profile/chirp/frame) to achieve a detection range of 200m (minimum 150m).
1. Configuration Requirements:
…
Hi Kazuya,
Thanks for reaching out again.
Selecting the Rsl = 0 will not effect the current limit. It is okay to use Rsl = 0, if the Duty cycle is not very large.
A small external RC filter (RF, CF) at the CS pin can be added to overcome the large…