Hi Jesse,
Please refer to the following thread regarding the HPF rough estimation could be plotted AWR1642BOOST: Range Resolution vs Spectral Resolution and SNR for Estimation of Range from Concrete Wall - Sensors forum - Sensors - TI E2E support forums…
Hi,
You can use the TI sensing estimator to determine the maximum range possible with a configuration. You can find the sensing estimator at the following location
https://dev.ti.com/gallery/view/mmwave/mmWaveSensingEstimator/ver/2.4.0/
You need…
Thank you for your reply.
Can changing the settings below solve the problem of the motor stalling due to the estimated BEMF being out of range?
Thanks.
Hi,
Because of imperfections in antenna layouts on the board, RF delays in SOC, etc, there is need to calibrate the sensor to compensate for bias in the range estimation and receive channel gain and phase imperfections. It's not completely necessary…
Hi Lakshmi-san,
I understand that. Because the audio signal level fluctuates depending on the input impedance value, I want to confirm whether that fluctuation falls within the acceptable range for input impedance. Therefore, I would appreciate it if…
Hi Diego,
We put sky651122 (FEM) to enhance power from 0dBm to 30dbm.
We don't see any improve from adjusting the following CCFG settings:
SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA = 0
SET_CCFG_MODE_CONF_XOSC_CAP_MOD = -128
Fullscreen…
Luke said: They are beginning to believe that their PCBA can become magnetized in a way that effects NFC communication. They have found some PCBAs that do not function as expected, where they only establish the NFC communication outside of the typical…
Part Number: IWR6843ISK Other Parts Discussed in Thread: MMWAVEICBOOST , , IWR6843AOPEVM , IWRL6432
Thank you very much for the incredibly clear and helpful guidance! Avoiding the DCA1000 and MMWAVEICBOOST significantly simplifies our experimental setup…
Hello Subhajit,
Thank you for the details.
When referring to changing the input (VG1) and RF/RG values, is the amplifier violating the input/output conditions? For this amplifier the input range is:
For a 10V single supply, input voltage must…
Abhishek,
Response for first case:
1. Your questions : The AD3552R eval board uses switches to configure gain, is this ok? Yes. This is a pretty common thing to do. You should take into account any on-resistance of the switch as it can effect gain…