Part Number: CS-AMPLIFIER-ERROR-TOOL Tool/software: Hi,
Hope you’re doing well. This is Sanjana Renganatha Desigan from Quantum Circuits, Inc. We are currently designing an RF front end and need advice for connectorized amplifiers that meet the requirements…
Hello,
Frank De Stasi said: The frequency can be either greater or less than nominal depending on how the tolerances stack up.
Considering the device's frequency accuracy (10%) and the tolerance of the external resistor, we estimate the frequency…
Hi Hogyun,
Please find the responses of your queries below:
About Q2,
I understand there are many parameters to consider of minimum received power.
Could you specify one case with any value fixed for the parameters?
Or let me know the formular…
hello Genatco,
Sorry for delayed reply, In our custom board PMSM is running fine. The estimated vales are consistent across multiple trials. We tested with different PMSM motors ranging from 110V-6A to 480V 14A. All PMSM motor are working well.
…
Part Number: AWR1843 Dear TI Support,
We are working with the AWR1843AOP and are seeing unexplained strong range artifacts on our custom PCB.
We have both the AWR1843AOPEVM and a custom PCB using the same radar device. To simplify the comparison,…
HI Jason,
I am unsure about the efficacy of adjusting the start time here. I believe the strong signal you are seeing at neat range is cause by the antenna coupling. We have provisions in the demo software which removes this signature. Please refer…
Part Number: IWR6843AOPEVM Other Parts Discussed in Thread: IWR6843AOP , IWRL6432AOP , IWRL6432AOPEVM , IWRL6432BOOST Hello,
I would like to compare and analyze the IWRL6432AOP and the IWR6843AOP. However, I found it difficult to make a clear comparison…
Part Number: TPS62442 Hi TI Support,
We are evaluating the TPS62442 for:
VIN: 5 V nominal, 5.5 V maximum
VOUT1: 0.75 V at ~1.1 A
VOUT2: 1.2 V at ~0.4 A
Forced PWM with external synchronization
We are considering a nominal 1.8 MHz external…
Part Number: TMS320F280037C Hello,
Firmware: UMCSDK v5.03 20kHz modulation
Busvoltage: +151v DC under full speed load
Is it possible to use vibration compenstaion module, VIB_COMP_A to reduce noise and torque ripple vibration for PMSM under FAST…